IMX6_L4.9.11_1.0.0_MFG_TOOL could not detect my device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6_L4.9.11_1.0.0_MFG_TOOL could not detect my device

844件の閲覧回数
heyitan
Contributor II

   I am working on my i.Mx6Q Sabre board and I found that the L4.9.11_1.0.0_MFG_TOOL could not detect my device, but the old versions such as L4.1.15 and L3.14.52 both work fine, could someone help me?

ラベル(2)
0 件の賞賛
2 返答(返信)

688件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Are you using the right vbs script for you board? And which flash are you want to download, SD card or EMMC?

Have a nice day

Rita

0 件の賞賛

687件の閲覧回数
heyitan
Contributor II

Hi

In fact I didn't read the MFG-TOOL user guide carefully, for earlier versions such as L4.1.15_MFG_TOOL and L3.14.52 versions , I just downloaded and unzipped the zip file, then I would do reconfigure the  cfg file to choose eMMC as my target flash, that always work. But when I did the same thing with the new version, I just failed in the first step, because when I connected my device , the tool remind me "No Device Connected".cfg.png

0 件の賞賛