IMX6 FCPBGA thermal interface pad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 FCPBGA thermal interface pad

Jump to solution
1,377 Views
sammypeiren
Contributor I

Hello,


I am designing a product that has an IMX6 processor in an FCPBGA package. The main PCB is mounted in an aluminum enclosure, which I would also like to use as a heatsink for the IMX6.

A thermal gap pad is placed between the enclosure and the IMX6 for optimal heat transfer. The pad is kept in place by the pressure of the case on the PCB. I have mechanical information about the pad (hardness, thickness, Young's Modulus), but I don't know how much pressure can be applied on the FCPBGA package.

Is there any information available from Freescale regarding about the maximum pressure that can be applied without damaging the package?

Labels (1)
0 Kudos
Reply
1 Solution
1,082 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sammy

maximum pressure is described on p.44 FCPBGA presentation

http://cache.freescale.com/files/32bit/doc/package_info/FC-PBGAPRES.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,083 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sammy

maximum pressure is described on p.44 FCPBGA presentation

http://cache.freescale.com/files/32bit/doc/package_info/FC-PBGAPRES.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,082 Views
sammypeiren
Contributor I

Alright so anything below 45N should be acceptable? I assume PoP versions of the IMX6 are a bit more fragile, or can they handle the same pressure?

0 Kudos
Reply