IMX6 EMMC从4.4换到5.1版无法烧录

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 EMMC从4.4换到5.1版无法烧录

3,640 次查看
jhp1234
Contributor I

有个问题 请问一下,原IM6的EMMC是SANDISK 4.41版,现在因为EMMC停产,EMMC换成5.1版的,按照官方的方法说是5.1版EMMC要降成4.41版来使用,修改了LTIB里的LINUX EMMC驱动:

/* workaround: support emmc 4.5 cards to work at emmc 4.4 mode */
if (card->ext_csd.rev > {
printk(KERN_ERR "%s: unrecognised EXT_CSD revision %d\n",
mmc_hostname(card->host), card->ext_csd.rev);
err = -EINVAL;
goto out;
}

生成uImage,放到Profiles\MX6Q Linux Update\OS Firmware下,但MFGTOOL一直卡在<CMD state="Updater" type="push" body="$ echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config">access boot partition 1</CMD>这一行 ,即显示access boot partition 1,不再往下执行,这种情况要怎么改?

0 项奖励
回复
9 回复数

3,631 次查看
jhp1234
Contributor I

CPU是IMX6Q, 用的LTIB L3.0.35_4.1.0, MFGTOOL也是对应的

0 项奖励
回复

3,637 次查看
jhp1234
Contributor I

EMMC驱动mmc.c修改了这里,完全按官方的方法改的

/* workaround: support emmc 4.5 cards to work at emmc 4.4 mode */
if (card->ext_csd.rev > {
printk(KERN_ERR "%s: unrecognised EXT_CSD revision %d\n",
mmc_hostname(card->host), card->ext_csd.rev);
err = -EINVAL;
goto out;
}

0 项奖励
回复

3,636 次查看
jhp1234
Contributor I

不知道为什么 > 8)不见了

0 项奖励
回复

3,616 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复

3,620 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you only need the modify the rev as we recommend, does it work well now?

0 项奖励
回复

3,601 次查看
jhp1234
Contributor I

I followed the method NXP recommanded, but the mfgtool can not work well, it always stops on   

"<CMD state="Updater" type="push" body="$ echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config">access boot partition 1</CMD>"

the mfgtool log error info:

ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ ls /dev/*
ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1024 count=16
ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config
ModuleID[2] LevelID[1]: PortMgrDlg(0)--MxHidDevice--Command Push(no file) excute failed

If cancel this command, mfgtool seems to write complete, but the device can not start.

Could you tell me why?

0 项奖励
回复

3,584 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you rebuild the the firmware uImage used for MfgTool ? You need to rebuild the uImage for Mfgtool, and then Update the uImage in Mfgtool .

0 项奖励
回复

3,580 次查看
jhp1234
Contributor I

Yes, I have, and replaced the uImage for mfgtool. 

0 项奖励
回复

3,593 次查看
jhp1234
Contributor I

the ucl2.xml :

<UCL>
<CFG>
<STATE name="BootStrap" dev="MX6Q" vid="15A2" pid="0054"/>
<STATE name="Updater" dev="MSC" vid="066F" pid="37FF"/>
</CFG>

<LIST name="SabreSD-eMMC" desc="Choose eMMC Linux as media">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot-mx6q-sabresd.bin" >Loading U-boot</CMD>
<CMD state="BootStrap" type="load" file="uImage" address="0x10800000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Loading Kernel.</CMD>
<CMD state="BootStrap" type="load" file="initramfs.cpio.gz.uboot" address="0x10C00000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Loading Initramfs.</CMD>
<CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>
<!-- UBOOT -->
<CMD state="Updater" type="push" body="$ ls /dev/*"/>
<CMD state="Updater" type="push" body="$ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1024 count=16">clean up u-boot parameter</CMD>
<CMD state="Updater" type="push" body="$ echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config">access boot partition 1</CMD>
<CMD state="Updater" type="push" body="send" file="files/u-boot.imx">Sending U-Boot</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=512 seek=2">write U-Boot to sd card</CMD>
<CMD state="Updater" type="push" body="$ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config">access user partition and enable boot partion 1 to boot</CMD>
<!-- KERNEL -->
<CMD state="Updater" type="push" body="send" file="files/kernel.bin">Sending kernel uImage</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=1M seek=1 conv=fsync">write kernel image to sd card</CMD>
<!-- make partition -->
<CMD state="Updater" type="push" body="send" file="mksdcard.sh.tar">Sending partition shell</CMD>
<CMD state="Updater" type="push" body="$ tar xf $FILE "> Partitioning...</CMD>
<CMD state="Updater" type="push" body="$ sh mksdcard.sh /dev/mmcblk0"> Partitioning...</CMD>
<CMD state="Updater" type="push" body="$ mkfs.ext4 -j /dev/mmcblk0p1">Formatting rootfs partition</CMD>
<CMD state="Updater" type="push" body="$ mkfs.ext4 -j /dev/mmcblk0p2">Formatting rootfs partition</CMD>
<!-- ROOT -->
<CMD state="Updater" type="push" body="$ mkdir -p /mnt/mmcblk0p1"/>
<CMD state="Updater" type="push" body="$ mount -t ext4 /dev/mmcblk0p1 /mnt/mmcblk0p1"/>
<CMD state="Updater" type="push" body="pipe tar -jxv -C /mnt/mmcblk0p1" file="files/rootfs.tar.bz2">Sending and writting rootfs</CMD>
<CMD state="Updater" type="push" body="frf">Finishing rootfs write</CMD>
<!-- SOFT -->
<CMD state="Updater" type="push" body="$ mkdir -p /mnt/mmcblk0p2"/>
<CMD state="Updater" type="push" body="$ mount -t ext4 /dev/mmcblk0p2 /mnt/mmcblk0p2"/>

<CMD state="Updater" type="push" body="$ mkdir -p /mnt/mmcblk0p2/firmware"/>
<CMD state="Updater" type="push" body="send" file="files/fpga.bin">Sending FPGA firmware </CMD>
<CMD state="Updater" type="push" body="$ cp $FILE /mnt/mmcblk0p2/firmware/fpga_firmware.bin">write FPGA firmware </CMD>

<CMD state="Updater" type="push" body="$ mkdir -p /mnt/mmcblk0p2/app"/>
<CMD state="Updater" type="push" body="pipe tar -jxv -C /mnt/mmcblk0p2/app" file="files/soft.tar.bz2">Sending and writting app</CMD>
<CMD state="Updater" type="push" body="frf">Finishing app write</CMD>

<CMD state="Updater" type="push" body="$ umount /mnt/mmcblk0p2">Unmounting config partition</CMD>
<CMD state="Updater" type="push" body="$ umount /mnt/mmcblk0p1">Unmounting rootfs partition</CMD>
<CMD state="Updater" type="push" body="$ echo Update Complete!">Done</CMD>
</LIST>

</UCL>

0 项奖励
回复