IMX6 Booting using SPI NAND FLASH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Booting using SPI NAND FLASH

1,242件の閲覧回数
shammi112
Contributor I

Hello.

Can i boot imx6 using SPI based NAND FLASH M29F4G01ADAGDSF-IT ?

Regards,

SHAMMI

0 件の賞賛
返信
3 返答(返信)

894件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SHAMMI

unfortunately boot from SPI based NAND is not supported by i.MX6DQ

according to boot options described in Chapter 8 System Boot i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

894件の閲覧回数
shammi112
Contributor I

hi,

Thanks for reply. Can be boot using MT29F128G08AJAAAWP  GPMI NAND FLASH, having 8k page size ?

Regards,

SHAMMI

0 件の賞賛
返信

894件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes, booting from parallel nands with 8k page size is supported.

~igor

0 件の賞賛
返信