hi all,
i am using imx535qsb board in that we include a camera interface application ov5640. we have captured the resolutions 640x480 and 720p video. when i tried to captured the 1080p video my application[mxc_v4l2_capture.c] does not supports it prints the following error message can anyone help me with this error message
ERROR:
root@freescale ~$ gst-launch mfw_v4lsrc fps-n=10 capture-width=1920 capture-heig
ht=1080 capture-mode=5 ! queue ! mfw_vpuencoder codec-type=0 ! avimux ! filesin
k location=shan3.avi sync=false
MFW_GST_V4LSRC_PLUGIN 2.0.3 build on Sep 29 2011 15:40:54.
(gst-launch-0.10:2252): GLib-GObject-WARNING **: value "1920" of type `gint' is invalid or out of range for property `capture-width' of type `gint'
Setting pipeline to PAUSED ...
[ALLOC] mem alloc cpu_addr = 0x0 Size 0x150b8
[INFO] Product Info: i.MX53
VPU Versi[ALLOC] mem alloc cpu_addr = 0x0 Size 0x100000
on: firmware 13.4.41; libvpu: 5.3.2
MFW_GST_VPU_ENCODER_PLUGIN 2.0.3 build on Sep 29 2011 15:40:26.
ERROR: v4l2 capture: width exceeds limit resize to 240.
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
Caught SIGSEGV accessing address 0x18
Spinning. Please run 'gdb gst-launch 2252' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.
hi daiane,
yes, i also checked the vpu specification. is there any chance to encode 1080p in imx535 qsb and this also need to my usecase
sorry for the delay , last four days i am out of station today only i came