IMX535 QSB 1080p video encoding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX535 QSB 1080p video encoding

1,198件の閲覧回数
shanmugamsundar
Contributor IV

hi all,

     i am using imx535qsb board in that we include a camera interface application ov5640. we have captured the resolutions 640x480 and 720p video. when i tried to captured the 1080p video my application[mxc_v4l2_capture.c] does not supports it prints the following error message can anyone help me with this error message

ERROR:


root@freescale ~$ gst-launch mfw_v4lsrc fps-n=10 capture-width=1920 capture-heig

ht=1080 capture-mode=5  ! queue ! mfw_vpuencoder codec-type=0 ! avimux ! filesin

k location=shan3.avi sync=false

MFW_GST_V4LSRC_PLUGIN 2.0.3 build on Sep 29 2011 15:40:54.

(gst-launch-0.10:2252): GLib-GObject-WARNING **: value "1920" of type `gint' is invalid or out of range for property `capture-width' of type `gint'

Setting pipeline to PAUSED ...

[ALLOC] mem alloc cpu_addr = 0x0  Size 0x150b8

[INFO]  Product Info: i.MX53

VPU Versi[ALLOC] mem alloc cpu_addr = 0x0  Size 0x100000

on: firmware 13.4.41; libvpu: 5.3.2

MFW_GST_VPU_ENCODER_PLUGIN 2.0.3 build on Sep 29 2011 15:40:26.

ERROR: v4l2 capture: width exceeds limit resize to 240.

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

Caught SIGSEGV accessing address 0x18

Spinning.  Please run 'gdb gst-launch 2252' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.


ラベル(2)
0 件の賞賛
7 返答(返信)

702件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

VPU encoding can go up to 720p@30 for some codecs. So you will not be able to encode 1080p stream. (I just double checked it on VPU specifications)

Does your usecase needs the encoding?

0 件の賞賛

702件の閲覧回数
shanmugamsundar
Contributor IV

hi daiane,

       yes, i also checked the vpu specification. is there any chance to encode 1080p in imx535 qsb and this also need to my usecase

     sorry for the delay , last four days i am out of station today only i came

0 件の賞賛

702件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I´ve never heard about 1080p encode on imx53.

Even if you was able to encode 1080p with qsb, i think it will not get a feasible performance.

0 件の賞賛

702件の閲覧回数
shanmugamsundar
Contributor IV

yes, you are correct we cant able to encode the 1080p video in imx qsb, we kept this process in hold. let see

Thanks

shan

0 件の賞賛

702件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

If 1080p encoding is needed, please consider mx6q.

Regards,

Fabio Estevam

0 件の賞賛

702件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Instead of encode it into a file. Are you able to preview it? (mfw_v4lsrc -> autovideosink)

0 件の賞賛

702件の閲覧回数
shanmugamsundar
Contributor IV

no i cant ,  Also i tried by taking the encoder in command but it remains same

Regards

shan

0 件の賞賛