I have some 1920x1080 screens attached by LVDS to a IMX53 platform. These needs to be rotated by 90 or 180°.
I'd prefere to do this in kernel space because I don't want the user to bother about the screen orientation.
Where do I start?
解決済! 解決策の投稿を見る。
In Linux BSP documentation package there's a document named "imx5x_IPU_LIB_UG.pdf". It describes IPU API and how you can use IPU to perform these functions accelerated by HW.
Usually your application will need to generate frame to a buffer of XxY size, and then you'd use IPU to rotate it to YxX framebuffer. So a small plugin is usually required to integrate to an existing app.
In Linux BSP documentation package there's a document named "imx5x_IPU_LIB_UG.pdf". It describes IPU API and how you can use IPU to perform these functions accelerated by HW.
Usually your application will need to generate frame to a buffer of XxY size, and then you'd use IPU to rotate it to YxX framebuffer. So a small plugin is usually required to integrate to an existing app.
Yes, but I want it in kernel, so that the user/app/whatever doesn't need to use the IPU api...
Hi wouter,
I'm in the need for rotating the FRAME buffer on the IMx53 .
Did you succeed in rotating ( so that bootup shows a correct display)?
Any pacthes requried ?
Regards
Noel
The user side library sits on top of kernel ioctl calls. You should be able to replicate the functionality kernel side that calls the IPU kernel driver functions directly.