IMX28 wince low power

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX28 wince low power

578 次查看
lee_ee
Contributor II

Dear all:

Dose the imx28 wince bsp supports STR(suspend-to-ram) function, how to implement it?

Thanks,

标签 (2)
0 项奖励
2 回复数

437 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lee

I am afraid it does not support, one can add such support using

linux sources (which supports it)

Board Support Packages (5)

i.MX28 Linux 2.6.35 Source Code Files and documentation (REV L2.6.35_1.1.0)

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励

437 次查看
lee_ee
Contributor II

Dear igor,

Thanks a lot for your support.

It's a pity that wince BSP does not support the STR function. I'm planning to implement low power consumption.

Kind Regards,

0 项奖励