IMX28 wince low power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX28 wince low power

621 Views
lee_ee
Contributor II

Dear all:

Dose the imx28 wince bsp supports STR(suspend-to-ram) function, how to implement it?

Thanks,

Labels (2)
0 Kudos
Reply
2 Replies

480 Views
igorpadykov
NXP Employee
NXP Employee

Hi lee

I am afraid it does not support, one can add such support using

linux sources (which supports it)

Board Support Packages (5)

i.MX28 Linux 2.6.35 Source Code Files and documentation (REV L2.6.35_1.1.0)

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

480 Views
lee_ee
Contributor II

Dear igor,

Thanks a lot for your support.

It's a pity that wince BSP does not support the STR function. I'm planning to implement low power consumption.

Kind Regards,

0 Kudos
Reply