Hi, everyone!
Now I‘m using imx 257 core board (OS for LINUX) of WEIM (external memory interface) 16 data synchronization (address 14), FPGA like an external memory to read and write, I used CS1 chip connected with FPGA the election, as the configuration of the drive:
mxc_request_iomux(MX25_PIN_A10, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_A13, MUX_CONFIG_FUNC); |
mxc_request_iomux(MX25_PIN_D0, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D1, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D2, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D3, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D4, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D5, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D6, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D7, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D8, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D9, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D10, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D11, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D12, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D13, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D14, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_D15, MUX_CONFIG_FUNC); |
mxc_request_iomux(MX25_PIN_EB0, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_EB1, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_OE, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_CS1, MUX_CONFIG_FUNC); | |
mxc_request_iomux(MX25_PIN_RW, MUX_CONFIG_FUNC); |
// | mxc_iomux_set_pad(MX25_PIN_A10, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_KEEPER ); |
mxc_iomux_set_pad(MX25_PIN_A13, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_KEEPER ); | |
mxc_iomux_set_pad(MX25_PIN_D0, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D1, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D2, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D3, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D4, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D5, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D6, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D7, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D8, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D9, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D10, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D11, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D12, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D13, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D14, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); | |
mxc_iomux_set_pad(MX25_PIN_D15, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST); |
mxc_iomux_set_pad(MX25_PIN_EB0, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL); | |
mxc_iomux_set_pad(MX25_PIN_EB1, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL); | |
mxc_iomux_set_pad(MX25_PIN_OE, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL); | |
// | |
mxc_iomux_set_pad(MX25_PIN_RW, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL); |
// | mxc_iomux_set_pad(MX25_PIN_CTL_GRP_DDRTYPE,0x0 << 11);//DDR_TYPE = 00 i don't know how to set the DDRTPYE |
// mxc_iomux_set_input(iomux_input_select_t input,u32 config)
//VA_ADDR = 0xFC522000
writel( 0x00001E00, VA_ADDR + 0x10);//CSCR1U | |
writel( 0xA0050841, VA_ADDR + 0x14);//CSCR1L | |
writel( 0x00005000, VA_ADDR + 0x18);//CSCR1A |
volatile unsigned long *eim_mem = NULL; | ||
eim_mem = (unsigned long*)ioremap(WEIM_CS1_BASE_ADDR, 0x4000); | // WEIM_CS1_BASE_ADDR 0xA8000000 | |
if(!eim_mem) | ||
{ | ||
printk("Failed to remap eim_mem\n"); | ||
} //write many times writew( 0x55aa, eim_mem); |
and there is no data on the CS1,anyone can help me?
Hi 志明 李
you can check if CCM clock is enabled for WEIM,
CGCR0 AHB Clock Gating[3] hclk_emi
As for Linux/Uboot one can look at i.MX35 PDK codes (it has parallel NOR)
IMX35_PDK_DESIGN_FILES: i.MX35 PDK
in particular weim mmu mapping in Uboot board_mmu_init().
Best regards
igor
connect jtag and check registers and try to write to WEIM directly,
also please check below
https://community.freescale.com/message/302947#302947
~igor