IMX257 communicate with FPGA by WEIM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX257 communicate with FPGA by WEIM

963 Views
bruce_lol
Contributor I

Hi, everyone!

    Now I‘m using imx 257 core board (OS for LINUX) of WEIM (external memory interface) 16 data synchronization (address 14), FPGA like an external memory to read and write, I used CS1 chip  connected with FPGA the election, as the configuration of the drive:

mxc_request_iomux(MX25_PIN_A10, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_A13, MUX_CONFIG_FUNC);

mxc_request_iomux(MX25_PIN_D0,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D1,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D2,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D3,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D4,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D5,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D6,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D7,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D8,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D9,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D10, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D11, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D12, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D13, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D14, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_D15, MUX_CONFIG_FUNC);

mxc_request_iomux(MX25_PIN_EB0, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_EB1, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_OE,  MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_CS1, MUX_CONFIG_FUNC);
mxc_request_iomux(MX25_PIN_RW,  MUX_CONFIG_FUNC);

//mxc_iomux_set_pad(MX25_PIN_A10, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_KEEPER );
mxc_iomux_set_pad(MX25_PIN_A13, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_KEEPER );
mxc_iomux_set_pad(MX25_PIN_D0,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D1,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D2,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D3,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D4,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D5,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D6,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D7,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D8,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D9,  PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D10, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D11, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D12, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D13, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D14, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);
mxc_iomux_set_pad(MX25_PIN_D15, PAD_CTL_HYS_CMOS|PAD_CTL_DRV_HIGH|PAD_CTL_PKE_ENABLE|PAD_CTL_100K_PU|PAD_CTL_ODE_CMOS|PAD_CTL_DRV_3_3V|PAD_CTL_PUE_KEEPER|PAD_CTL_SRE_FAST);

mxc_iomux_set_pad(MX25_PIN_EB0, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL);
mxc_iomux_set_pad(MX25_PIN_EB1, PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL);
mxc_iomux_set_pad(MX25_PIN_OE,  PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL);
//
mxc_iomux_set_pad(MX25_PIN_RW,  PAD_CTL_DRV_HIGH|PAD_CTL_PUE_PULL);

//mxc_iomux_set_pad(MX25_PIN_CTL_GRP_DDRTYPE,0x0 << 11);//DDR_TYPE = 00 i don't know how to set the DDRTPYE

// mxc_iomux_set_input(iomux_input_select_t input,u32 config)

//VA_ADDR = 0xFC522000

writel( 0x00001E00, VA_ADDR + 0x10);//CSCR1U
writel( 0xA0050841, VA_ADDR + 0x14);//CSCR1L
writel( 0x00005000, VA_ADDR + 0x18);//CSCR1A

volatile unsigned long *eim_mem = NULL;
eim_mem = (unsigned long*)ioremap(WEIM_CS1_BASE_ADDR, 0x4000);
// WEIM_CS1_BASE_ADDR 0xA8000000
if(!eim_mem)
{
    printk("Failed to remap eim_mem\n");

}

//write many times

writew( 0x55aa, eim_mem);

and there is no data on the CS1,anyone can help me?

Labels (1)
0 Kudos
3 Replies

684 Views
igorpadykov
NXP Employee
NXP Employee

Hi 志明 李

you can check if CCM clock is enabled for WEIM,

CGCR0 AHB Clock Gating[3] hclk_emi

As for Linux/Uboot one can look at i.MX35 PDK codes (it has parallel NOR)

IMX35_PDK_DESIGN_FILES: i.MX35 PDK

L2.6.31_09.12.01_SDK_SOURCE

in particular weim mmu mapping in Uboot board_mmu_init().

Best regards

igor

0 Kudos

684 Views
bruce_lol
Contributor I

Hi,thks for the reply,I check the emi clk is enable

0 Kudos

683 Views
igorpadykov
NXP Employee
NXP Employee

connect jtag and check registers and try to write to WEIM directly,

also please check below

https://community.freescale.com/message/302947#302947

~igor

0 Kudos