hello,
Am IMX28 EVK and Linux BSP 2.6.35... I tried following this pdf and developing a UART test code
http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf
But when i tried the command ./uart_appnote /dev/ttymxc2 i found that /dev/ttymxc2 is missing there is no ttymxc0 or ttymxc1.
So How can i get the UART device files. Do i need to edit source files or is there any configuration missing in BSP building
Thanks gonfer
But when i tried that ttySP2
root@freescale /home/user$ ./uart_appnote /dev/ttySP2
Test: MXC UART With Eclipse !
Usage: mxc_uart_test <UART device name, opens UARmxs-auart mxs-auart.2: Unhandled status 52028d
T2 if no dev name is specified>
/dev/ttySP2 opened
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back=
I got this reply..there is no Data Read back??
Hi gonfer,
Source code
#include <stdio.h>
#include <stdlib.h>
#include <sys/types.h>
#include <sys/stat.h>
#include <fcntl.h>
#include <termios.h>
#include <sys/ioctl.h>
#include <unistd.h>
#define LOOPBACK 0x8000
int main(int argc, char **argv)
{
int uart_file1;
unsigned int line_val;
char buf[5];
struct termios mxc, old;
int retval;
printf("Test: MXC UART With Eclipse !\n");
printf("Usage: mxc_uart_test <UART device name, opens UART2 if no dev name is specified>\n");
if (argc == 1) {
/* No Args, open UART 2 */
if ((uart_file1 = open("/dev/ttymxc/1", O_RDWR)) == -1) {
printf("Error opening UART 2\n");
exit(1);
} else {
printf("Test: UART 2 opened\n");
}
} else {
/* Open the specified UART device */
if ((uart_file1 = open(*++argv, O_RDWR)) == -1) {
printf("Error opening %s\n", *argv);
exit(1);
} else {
printf("%s opened\n", *argv);
}
}
tcgetattr(uart_file1, &old);
mxc = old;
mxc.c_lflag &= ~(ICANON | ECHO | ISIG);
retval = tcsetattr(uart_file1, TCSANOW, &mxc);
printf("Attributes set\n");
line_val = LOOPBACK;
ioctl(uart_file1, TIOCMSET, &line_val);
printf("Test: IOCTL Set\n");
write(uart_file1, "Test\0", 5);
printf("Data Written= Test\n");
read(uart_file1, buf, 5);
printf("Data Read back= %s\n", buf);
sleep(2);
ioctl(uart_file1, TIOCMBIC, &line_val);
retval = tcsetattr(uart_file1, TCSAFLUSH, &old);
close(uart_file1);
return 0;
}
hello gonfer,
I got the return values as zero
root@freescale /home/user$ ./uart_appnote /dev/ttySP2
Test: MXC UART With Eclipse !
Usage: mxmxs-auart mxs-auart.2: Unhandled status 52028d
c_uart_test <UART device name, opens UART2 if no dev name is specified>
/dev/ttySP2 opened
The first retval is 0
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back=
The second retval is 0
Hi Ganesh,
I think I've found 2 problems:
1st one:
#define LOOPBACK 0x8000
I think this value goes into HW_UARTAPP_CTRL2 register, and its purpose is to activate LBE bit. If this is so, then LOOPACK should be defined as 0x0080.
2nd one:
I've taken a quick look to the application uart driver and it looks that setting the LBE bit is not supported, so you should modify this driver to support this feature.
I've brute forced the driver setting always the LBE bit and the source code you have posted runs fine.
Regards,
Gonzalo.
Hi Ganesh,
a deeper look shows I was wrong - the name LOOPBACK was misleading me, but the definition is OK. I think a more appropriate name could be use, like:
#define TIOCM_LOOP 0x8000
like in kernel headers.
To add support for the LOOPBACK feature in the driver (not brute forcing):
1.- In /arch/arm/mach-stmp378x/include/mach/regs-uartapp.h you should add:
#define BM_UARTAPP_CTRL2_LBE 0x00000080
2.- In /drivers/serial/mxs-auart.c look for static void mxs_auart_set_mctrl(struct uart_port *u, unsigned mctrl). This function should look something like this:
static void mxs_auart_set_mctrl(struct uart_port *u, unsigned mctrl)
{
struct mxs_auart_port *s = to_auart_port(u);
u32 ctrl = __raw_readl(u->membase + HW_UARTAPP_CTRL2);
ctrl &= ~(BM_UARTAPP_CTRL2_RTS | BM_UARTAPP_CTRL2_LBE);
if (mctrl & TIOCM_RTS)
ctrl |= BM_UARTAPP_CTRL2_RTS;
if (mctrl & TIOCM_LOOP)
ctrl |= BM_UARTAPP_CTRL2_LBE;
s->ctrl = mctrl;
__raw_writel(ctrl, u->membase + HW_UARTAPP_CTRL2);
}
Then, recompile the kernel and you are done. I've ran your code in my iMX28evk and works fine !!
Regards,
Gonzalo.