IMX 25 WinCE 6.0 Bootloader for NAND flash.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX 25 WinCE 6.0 Bootloader for NAND flash.

1,610 次查看
aswinpp
Contributor I

Hi All,

     I am a newbie on imx platform and unfortunately i lost the preloaded WinCE 6.0 Bootloader in NAND flash.

So I can't boot the device.

I tried to program Eboot.nb0 and XLDR.nb0 to NAND as well as SD Card using ATK, B@@ut its not loading Bootloaders.

Can anybody give me the correct procedure to program bootloader to NAND and SD Card.. Also provide Working Bootloader binaries for WinCE6.0 IMX25 platform.

Thanks and Regards

Aswin

标签 (2)
0 项奖励
1 回复

965 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ASWIN

please look below

IMX25_WINCE600_DEMOFILES_09_12  : 2009.12 Windows Embedded CE 6.0 Demo Images.

IMX25_PDK09_12_WIN60DOCS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励