Hi,
We want to use IEEE 1588 feature on i.MX6Q Gigabit Ethernet MAC. I have two questions:
1. We need i.MX6Q output 1pps signal. Which pin of the i.MX6Q can be used to output the 1pps? Can we use ENET_1588_EVENTx_OUT?
2. We need i.MX6Q ENET output 50MHz clock so that devices connected to the 1pps and 50MHz clock can get precise timestamp. Can ENET_1588_EVENTx_OUT be used as 50MHz clock output?
Thanks!
Hello,
The following thread clarifies the issue.
ENET-1588 PTP with hardware timestamp
For more information please refer to section "How to Use the Stacks in Linux OS" in
"ENET IEEE-1588 Driver" chapter of "i.MX_Linux_Reference_Manual.pdf".
Also, note : to activate PPS on master the phc2sys should be run with ptp4l.
http://events.linuxfoundation.org/sites/events/files/slides/lcjp14_ichikawa_0.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------