IEEE 1588 clock synchronization for multi-ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IEEE 1588 clock synchronization for multi-ports

865件の閲覧回数
mingzheliu
Contributor I

Hi,

I am using IMXRT1064 to implement IEEE 1588 function on two Ethernet ports simultaneously. So I need them to have a common reference timer. I saw in the manual that I can enable timer slave mode (ENETn_ATCR [SLAVE] = 1). By enabling slave mode (ENETn_ATCR[SLAVE] = 1), the timer is ignored and the current time is externally provided from one of the external modules.

How should I use it?

Thank you.

ラベル(1)
0 件の賞賛
2 返答(返信)

777件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mingzhe Liu,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the application note:
https://www.nxp.com/docs/en/nxp/application-notes/AN12149.pdf for details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

777件の閲覧回数
mingzheliu
Contributor I

Hi,

Thank you for your reply. I had seen the documentation of that you said. But I didn't find any explanation about "slave mode" in the AN12149.pdf.

There is a short description in section 41.7.10.2 of IMXRT1064RM.pdf. But I didn't know how to configurate it.

Here is the description:

0 件の賞賛