I2S Driver in FreeRTOS package of the imx7s architecture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2S Driver in FreeRTOS package of the imx7s architecture

ソリューションへジャンプ
1,091件の閲覧回数
vivekrajpara
Contributor III

Hi All,

I am working on imx7s architecture which has Cortex M4 and Cortex A7 in it.

I am using development board which has SGLT500 audio code.I am trying to capture I2S data from Cortex M4 core. Can anyone point out what would be the best way to do it or if driver for I2S available for FreeRTOS on Imx.7s?

Thank you in advance

Vivek

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
729件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vivek

I am not aware of i.MX7 I2S driver for FreeRTOS however

one can look at kinetis example

https://community.nxp.com/thread/81904#81904 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
730件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vivek

I am not aware of i.MX7 I2S driver for FreeRTOS however

one can look at kinetis example

https://community.nxp.com/thread/81904#81904 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

729件の閲覧回数
vivekrajpara
Contributor III

Thank you Igor for quick reply.

0 件の賞賛