We have a RTC/NVRAM (PCF2127a) chip on the i2C bus. We have seen a few rare occasions where it is not detected during boot (but is detect on another boot). Is there a way for me to force a re-probe if we don't see the device after we boot up?
To help debug this issue we have put a switch on the data line, so I can force a failure at boot. But I still can't talk to the chip afterwards because the part wasn't detected.
This is on an iMX35 on 2.6.31 kernel. The device driver is built in, I don't believe its in a module.
i2c-adapter i2c-0: IRQ: Bus Arbitration lost
i2c-adapter i2c-0: Could not grab Bus ownership
WARNING: i2c bus failed. RTC is not itialized or registered
rtc-pcf2127a: probe of 0-0051 failed with error -121
i2c /dev entries driver
seems it is not stable during boot. Have you try to build it as module and then load it automatically after boot?
I haven't, but I will give that a try when I can. Other fires are hotter right now.