I

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
691 次查看
cyrusvali
Contributor II

Hi

I have a question about ARM architecture

why there is two registers to enable/disable interrupts? ISER and ICER

Is it not possible to set/reset the same register for enable/disabling the interrupts?

thank you

1 解答
584 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Cyrus,

this question is related to ARM Cortex processor rather that the whole NXP MCU. For instance you should identify which ARM core are you using. For details about ARM cores you may contact ARM or check their infocenter.

4.2.3. Interrupt Clear-enable Register

4.2.2. Interrupt Set-enable Registers


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
585 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Cyrus,

this question is related to ARM Cortex processor rather that the whole NXP MCU. For instance you should identify which ARM core are you using. For details about ARM cores you may contact ARM or check their infocenter.

4.2.3. Interrupt Clear-enable Register

4.2.2. Interrupt Set-enable Registers


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------