I cannot get Ethernet working on my 4.9.11 kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I cannot get Ethernet working on my 4.9.11 kernel

1,974 次查看
dougbailey
Contributor III

I have a board based on the Freescale iMX6DL SabreSD design that I have working fine with the Korgoth based BSP that runs Linux 4.1.15. I am trying to upgrade the BSP running on the board to the Morty based BSP that runs Linux 4.9.11.

The design uses the Micrel KSZ8081RNACA PHY in a RMII configuration where the PHY is driving the 50 MHz reference clock.

I can run the Ethernet link with no problems using the 4.1.15 kernel. However, I am having issues getting the Ethernet on the 4.9.11 kernel to handle packets. I can never get packets in or out of the Ethernet link.

I can bring the link up using the iproute2 commands (e.g. ip link set dev eth1 up) and see the link come up and report that it is active. I am able to communicate with the PHY via MDIO and it reports that has a valid link and negotiates to a 100 Mb/s stream.

When I use a scope to look at the CRS_DV signal, I see a valid detection of incoming packets. (The signal looks the same for both the 4.1.15 and 4.9.11 kernels.) However, I never see the interrupt activated for the incoming RX Buffer.


IOMuxC for the CRS_DV signal which is connected to the ENET_CRS_DV pin.
=======================================================================
IOMUXC_SW_MUX_CTL_PAD_ENET_CRS_DV
0x020E01E4 = 0x00000001
ALT1 — Select signal ENET_RX_EN.

IOMUXC_ENET_MAC0_RX_EN_SELECT_INPUT
0x020E0828 = 0x00000000
(ENET_CRS_DV_ALT1 — Selecting ALT1 mode of pad ENET_CRS_DV for ENET_RX_EN.)

IOMUXC_SW_PAD_CTL_PAD_ENET_CRS_DV
0x020E05B4 = 0x000130B0


IOMuxC for the RMII Reference Clock input on GPIO16.
====================================================
IOMUXC_SW_MUX_CTL_PAD_GPIO16
0x020E0214 = 0x00000002
ALT2 — Select signal ENET_REF_CLK.

IOMUXC_ENET_REF_CLK_SELECT_INPUT
0x020E080C = 0x00000000
GPIO16_ALT2 — Selecting ALT2 mode of pad GPIO_16 for ENET_REF_CLK.

IOMUXC_SW_PAD_CTL_PAD_GPIO16
0x020E05E4 = 0x0001B0B0


FEC Ethernet Registers:
======================
Interrupt Mask Register (ENET_EIMR)
0x02188008 = 0x0A8080AA
Enabled Interrupts: TXF, RXF, MII, TS_TIMER

(Note: I only see the MII interrupt handled. )

Ethernet Control Register (ENET_ECR)
0x02188024 = 0xF0000112
10/100 mode, MAC is enabled, and reception and transmission are possible.

Receive Control Register (ENET_RCR)
0x02188084 = 0x45F20124
RMII Mode, Frame len 1522 bytes
(Note I tried both promiscuous and non-promiscuous mode with the same result)

Rx Packet Count Statistic Register (ENET_RMON_R_PACKETS)
0x2188284 = 0


The devicetree set up I am using is as follows:

&fec {
  pinctrl-names = "default";
  pinctrl-0 = <&pinctrl_enet>;
  phy-mode = "rmii";
  phy-reset-gpios = <&gpio1 2 0>;
  phy-reset-duration = <10>;
  fsl,magic-packet;
  status = "okay";
};
soc {
  aips-bus@02100000 {
    fec: ethernet@02188000 {
      compatible = "fsl,imx6q-fec";
      reg = <0x02188000 0x4000>;
      interrupts-extended =
            <&gpc 0 118 IRQ_TYPE_LEVEL_HIGH>,
            <&gpc 0 119 IRQ_TYPE_LEVEL_HIGH>;
      clocks = <&clks IMX6QDL_CLK_ENET>,
            <&clks IMX6QDL_CLK_ENET>,
            <&clks IMX6QDL_CLK_ENET_REF>;
      clock-names = "ipg", "ahb", "ptp";
      stop-mode = <&gpr 0x34 27>;
      fsl,wakeup_irq = <0>;
      status = "disabled";
    };
  };
};


&iomuxc {
  pinctrl_enet: enetgrp {
      fsl,pins = <
            MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0
            MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0
            MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0 0x1b0b0
            MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x1b0b0
            MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x1b0b0
            MX6QDL_PAD_GPIO_16__ENET_REF_CLK 0x1b0b0
            MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0 0x1b0b0
            MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1 0x1b0b0
            MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN 0x130b0
            MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER 0x1b0b0
            MX6QDL_PAD_GPIO_2__GPIO1_IO02 0x1b0b0
      >;
  };

};

Since the Ethernet works with the 4.1.15 kernel, I am assuming that I am just not setting something up correctly in the 4.9 kernel.

Does anyone have any suggestions as to where I can look that can give me an indication as to why I am not seeing any incoming packets? Are there any decent app notes describing what is required for the Fast Ethernet Controller's initialization?

Regards, 

Doug Bailey

标签 (2)
0 项奖励
4 回复数

1,152 次查看
dougbailey
Contributor III

It turns out that my problem is the ENET_CLK_SEL bit in the IOMUXC_GPR1 register.  This was causing contention on the reference clock line. 

I have not seen a way to clear this bit via the device tree.  Anybobdy know the magic formula? 

0 项奖励

1,152 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Doug

one can add IOMUXC_GPR1 configuration in uboot board file (./mx6sabresd/mx6sabresd.c), as

for dts one can look in fec source file described in attached Linux Manual sect.4.5 Fast Ethernet

Controller (FEC), seems there is no such setting.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,152 次查看
dougbailey
Contributor III

Unfortunately, the bit is set actively in the kernel initialization.  

The following fragment sets the bit ./arch/arm/mach-imx/mach-imx6q.c

/*
* If enet_ref from ANATOP/CCM is the PTP clock source, we need to
* set bit IOMUXC_GPR1[21]. Or the PTP clock must be from pad
* (external OSC), and we need to clear the bit.
*/
gpr = syscon_regmap_lookup_by_compatible("fsl,imx6q-iomuxc-gpr");
if (!IS_ERR(gpr))
    regmap_update_bits(gpr, IOMUXC_GPR1,
        IMX6Q_GPR1_ENET_CLK_SEL_MASK,
        IMX6Q_GPR1_ENET_CLK_SEL_ANATOP);
    else
        pr_err("failed to find fsl,imx6q-iomuxc-gpr regmap\n");

Regards, 

Doug 

0 项奖励

1,152 次查看
dougbailey
Contributor III

My solution was to change:

regmap_update_bits(gpr, IOMUXC_GPR1,
        IMX6Q_GPR1_ENET_CLK_SEL_MASK,
        IMX6Q_GPR1_ENET_CLK_SEL_ANATOP);

to 

regmap_update_bits(gpr, IOMUXC_GPR1,
        IMX6Q_GPR1_ENET_CLK_SEL_MASK,
        IMX6Q_GPR1_ENET_CLK_SEL_PAD);

0 项奖励