Hi,
I'm actually try to boot on NAND of my IMX28 EVK board but when I search mtd0 or else on /dev/ on my board, I can't find anyone. I have a lot of tty, pty, but not them. Udev and mtd-utils in ltib are checked. I think my configuration is bad but i don't know where is wrong. My question is how to find or configure them?
Thanks in advance
PS: This is my linux.conf
Original Attachment has been moved to: linux.config.zip
已解决! 转到解答。
Sorry, I am a bit confused. Your initial question was about NAND, then you switched to CAN.
The mx28evk does not come with a NAND chip populated, but if you populate a NAND chip into the slot and pass 'gpmi' you should be able to see the NAND getting detected in the kernel log.
And this might be helpfull if you use the patch and want to use the CAN with canutils
https://community.freescale.com/docs/DOC-1437
I Just made it wok today, I can go back home for the weekend :smileyhappy:
Thanks for the help. I try for the CAN and I realise I have already try this but when I didn't seen /dev/can0 or else, I through the CAN didn't work but now I try to listen and after to send a message and it work. I'm so sad, the answer was so close ^^
For the NAND my problem is not on the boot, it's before that. In /dev, I don't have mtd0 ... or mtdblock0... so when I want to erase or write on the NAND I can't and I have this message
root@imx28 /$ flash_eraseall /dev/mtd0
flash_eraseall: /dev/mtd0: No such file or directory
if I cat /proc/mtd I have no partition
root@imx28 /$ cat /proc/mtd
dev: size erasesize name
root@imx28 /$
I can create the port manually but I don't know how to make the link to the hardware.
Regards
Mickael
1/ On evaluation board, there is a dipswitch S2 to choose your boot mode : see "§2.3 Boot Mode" in
IMX28EVKHUG.pdf. Have you tried that?
2/ For the CAN stuff :
• Modifying bitrate :
$ echo 250000 > /sys/devices/platform/FlexCAN.0/bitrate
• Read bitrate :
$ cat /sys/devices/platform/FlexCAN.0/bitrate
• CAN activation on « can0 » :
$ ip link set can0 up
• Sending message
$ cantest can0 ‘71E#DEADBEEF’
• Witing for message
$ cantest can0 &
To deploy cantest :
./ltib -m prep -p cantest
./ltib -m scbuild -p cantest.spec
./ltib -m scinstall -p cantest.spec
./ltib -m scdeploy -p cantest.spec
Then: sudo scp rootfs/usr/bin/cantest root@192.168.1.25:/usr/bin
But FYI, there is a bug in the driver :
https://community.freescale.com/message/273094#273094
Hope it helps...
Hi, thanks for reply
Yes I try but nothing change. I noticed that my port can0 and can1 are not here too but when I search on my board in /sys/devices/platform and I found FlexCAN.0 and FlexCAN.1. I try to see the difference between FlexCAN.0 and mxs-auart.1 per example and I realise the directory tty with the name of the port inside is missing(I don't know if I was clear) and I don't know how to change that.
I change a few option in my kernel to activate NAND like describe in i.MX28_Linux_BSP_RM.pdf part 14.4 and this my linux.conf now.
Best regards
Mickael
Sorry, I am a bit confused. Your initial question was about NAND, then you switched to CAN.
The mx28evk does not come with a NAND chip populated, but if you populate a NAND chip into the slot and pass 'gpmi' you should be able to see the NAND getting detected in the kernel log.
Sorry for that, I found the problem of my CAN after the NAND and when I didn't seen both of port, I thought it was the same problem, but no. I'm a little dumb because in the NAND socket there is no NAND and I don't realize that.
Thanks to both of you for your replies, that help me very much.
Regards
Mickael