I.MX7 Flashing Linux by uuu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX7 Flashing Linux by uuu

665 Views
mrshafie
Contributor II

hi.

I want to flash linux bsp using uuu on I.MX7 SABRESD board . so I download L4.9.88_2.0.0_images_MX6UL7D.tar.gz from NXP Community. 

for this end I wrote this uuu file:

#=============================================

uuu_version 1.2.39

SDP: boot -f bsp/L4.9.88_2.0.0_images_MX6UL7D/u-boot-imx7dsabresd_sd.imx
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all bsp/fsl-image-validation-imx-xwayland-imx6ul7d.sdcard
FB: flash bootloader bsp/L4.9.88_2.0.0_images_MX6UL7D/u-boot-imx7dsabresd_sd.imx
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done

#===============================

I use u-boot-imx7dsabresd_sd.imx and linux image from L4.9.88_2.0.0_images_MX6UL7D.tar.gz package. but this is output:

#============== output

.

.

Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args; if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_a;
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!

#===========

can any body help me? how to flash linux on i.mx7d using uuu? 

Thanks for your attention.

0 Kudos
Reply
1 Reply

655 Views
igorpadykov
NXP Employee
NXP Employee

Hi mrshafie

 

for old releases like L4.9.88_2.0.0, mfg tool was used (not uuu) for

programming images:  Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX6,7 BSP

https://www.nxp.com/design/software/embedded-software/i-mx-software:IMX-SW

use for example mfgtool2-yocto-mx-sabresd-emmc2(mx7d).vbs script included in

package.

In last linux released uuu sample scripts are already included in demo images, /samples folder.

 

Best regards
igor

0 Kudos
Reply