I.MX6ULL run IAR project download error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX6ULL run IAR project download error

743 次查看
刘卫强刘
Contributor I

I.MX6ULL run IAR project  download error

I use SDK_2.2_MCIM6ULL_RFP_Win.exe to generate sdk package  named  SDK_2.2_MCIM6ULL,run the  hello_world demo use IAR, at  the ddr_debug is ok, run normal, but in the debug modle is error,the debug log is below:

I have made the corresponding changes in accordance with the requirements of the manual (MCUXpresso SDK Release Notes for i.MX 6ULL Devices.pdf), but still can't run.

  • Set boot mode to reserved mode (BMODE[1:0]=2'b11).
  • Run mfgtool2-erase-sdk20-mx6ul-evk-qspi-nor-n25q256a.vbs to erase QSPI flash or run mfgtool2-erase-sdk20-mx6ulevk-sdcard.vbs to clear image vector table in MicroSD card before using IAR.

 

What should I do to make the demo work in debug mode?  ths!

  

the debug log :

Wed Sep 19, 2018 22:23:52: IAR Embedded Workbench 7.80.4 (armproc.dll)
Wed Sep 19, 2018 22:23:52: Device "CORTEX-A7" selected.
Wed Sep 19, 2018 22:23:52: JLINK command: ProjectFile = C:\NXP\SDK_2.2_MCIM6ULL\boards\evkmcimx6ull\demo_apps\hello_world\iar\settings\hello_world_Debug.jlink, return = 0
Wed Sep 19, 2018 22:23:52: JLINK command: scriptfile = C:\NXP\SDK_2.2_MCIM6ULL\boards\evkmcimx6ull\demo_apps\hello_world\iar/../ddr_init.jlinkscript, return = 0
Wed Sep 19, 2018 22:23:52: Device "CORTEX-A7" selected.
Wed Sep 19, 2018 22:23:52: DLL version: V6.12f, compiled Jan 13 2017 16:37:50
Wed Sep 19, 2018 22:23:52: Firmware: J-Link ARM V8 compiled Nov 28 2014 13:44:46
Wed Sep 19, 2018 22:23:52: JTAG speed is initially set to: 32 kHz
Wed Sep 19, 2018 22:23:52: Initial reset was performed
Wed Sep 19, 2018 22:23:52: Config JTAG Speed to 4000kHz
Wed Sep 19, 2018 22:23:52: TotalIRLen = 13, IRPrint = 0x0101
Wed Sep 19, 2018 22:23:52: Warning: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet = 2)
Wed Sep 19, 2018 22:23:52: ARM AP[0]: 0x74770001, AHB-AP
Wed Sep 19, 2018 22:23:52: ARM AP[1]: 0x44770002, APB-AP
Wed Sep 19, 2018 22:23:52: ROMTbl 0 [0]: 00001003, CID: B105900D, PID:04-001BB961 TMC
Wed Sep 19, 2018 22:23:52: ROMTbl 0 [1]: 00002003, CID: B105900D, PID:04-004BB906 ECT / CTI
Wed Sep 19, 2018 22:23:52: ROMTbl 0 [2]: 00003003, CID: B105900D, PID:04-004BB912 TPIU
Wed Sep 19, 2018 22:23:52: ROMTbl 0 [3]: 00004003, CID: B105F00D, PID:04-001BB101
Wed Sep 19, 2018 22:23:52: ROMTbl 0 [4]: 00020003, CID: B105100D, PID:04-000BB4A7 ROM Table
Wed Sep 19, 2018 22:23:52: ROMTbl 1 [0]: 00010003, CID: B105900D, PID:04-005BBC07 Cortex-A7
Wed Sep 19, 2018 22:23:52: Found Cortex-A7 r0p5
Wed Sep 19, 2018 22:23:52: 6 code breakpoints, 4 data breakpoints
Wed Sep 19, 2018 22:23:52: Debug architecture ARMv7.1
Wed Sep 19, 2018 22:23:52: Data endian: little
Wed Sep 19, 2018 22:23:52: Main ID register: 0x410FC075
Wed Sep 19, 2018 22:23:52: I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
Wed Sep 19, 2018 22:23:52: D-Cache L1: 32 KB, 128 Sets, 64 Bytes/Line, 4-Way
Wed Sep 19, 2018 22:23:52: Unified-Cache L2: 128 KB, 256 Sets, 64 Bytes/Line, 8-Way
Wed Sep 19, 2018 22:23:52: System control register:
Wed Sep 19, 2018 22:23:52: Instruction endian: little
Wed Sep 19, 2018 22:23:52: Level-1 instruction cache disabled
Wed Sep 19, 2018 22:23:52: Level-1 data cache disabled
Wed Sep 19, 2018 22:23:52: MMU disabled
Wed Sep 19, 2018 22:23:52: Branch prediction enabled
Wed Sep 19, 2018 22:23:52: Enabling i.MX6ULL DDR3L
Wed Sep 19, 2018 22:23:52: Clock Init Done
Wed Sep 19, 2018 22:23:53: DDR Init Done
Wed Sep 19, 2018 22:23:53: Found 3 JTAG devices, Total IRLen = 13:
Wed Sep 19, 2018 22:23:53: #0 Id: 0x5BA00477, IRLen: 4, IRPrint: 0x1 CoreSight JTAG-DP
Wed Sep 19, 2018 22:23:53: #1 Id: 0x00000001
Wed Sep 19, 2018 22:23:53: #2 Id: 0x088C101D
Wed Sep 19, 2018 22:23:53: 9808 bytes downloaded and verified (15.70 Kbytes/sec)
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002000, target byte: 0x00, byte in file: 0x18
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002001, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002002, target byte: 0x00, byte in file: 0x9F
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002003, target byte: 0x00, byte in file: 0xE5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002004, target byte: 0x00, byte in file: 0x18
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002005, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002006, target byte: 0x00, byte in file: 0x9F
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002007, target byte: 0x00, byte in file: 0xE5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002008, target byte: 0x00, byte in file: 0x18
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002009, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000200A, target byte: 0x00, byte in file: 0x9F
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000200B, target byte: 0x00, byte in file: 0xE5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000200C, target byte: 0x00, byte in file: 0x18
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000200D, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000200E, target byte: 0x00, byte in file: 0x9F
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000200F, target byte: 0x00, byte in file: 0xE5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002010, target byte: 0x00, byte in file: 0x18
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002011, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002012, target byte: 0x00, byte in file: 0x9F
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002013, target byte: 0x00, byte in file: 0xE5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002018, target byte: 0x00, byte in file: 0x14
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002019, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000201A, target byte: 0x00, byte in file: 0x9F
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000201B, target byte: 0x00, byte in file: 0xE5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000201C, target byte: 0x00, byte in file: 0x14
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000201D, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000201E, target byte: 0x00, byte in file: 0x9F
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000201F, target byte: 0x00, byte in file: 0xE5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002020, target byte: 0x00, byte in file: 0xD4
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002021, target byte: 0x00, byte in file: 0x3C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002023, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002024, target byte: 0x00, byte in file: 0x68
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002025, target byte: 0x00, byte in file: 0x3C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002027, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002028, target byte: 0x00, byte in file: 0x6C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002029, target byte: 0x00, byte in file: 0x3C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000202B, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000202C, target byte: 0x00, byte in file: 0x70
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000202D, target byte: 0x00, byte in file: 0x3C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000202F, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002030, target byte: 0x00, byte in file: 0x74
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002031, target byte: 0x00, byte in file: 0x3C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002033, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002034, target byte: 0x00, byte in file: 0x78
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002035, target byte: 0x00, byte in file: 0x3C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002037, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002038, target byte: 0x00, byte in file: 0xCC
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002039, target byte: 0x00, byte in file: 0x3C
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000203B, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002040, target byte: 0x00, byte in file: 0x2D
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002041, target byte: 0x00, byte in file: 0xE9
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002042, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002043, target byte: 0x00, byte in file: 0x41
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002044, target byte: 0x00, byte in file: 0x04
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002046, target byte: 0x00, byte in file: 0x0D
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002048, target byte: 0x00, byte in file: 0x24
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002049, target byte: 0x00, byte in file: 0xB2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000204A, target byte: 0x00, byte in file: 0x26
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000204B, target byte: 0x00, byte in file: 0x0A
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000204C, target byte: 0x00, byte in file: 0x24
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000204D, target byte: 0x00, byte in file: 0xB2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000204E, target byte: 0x00, byte in file: 0x60
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002050, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002051, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002052, target byte: 0x00, byte in file: 0x1E
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002053, target byte: 0x00, byte in file: 0x07
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002054, target byte: 0x00, byte in file: 0x07
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002055, target byte: 0x00, byte in file: 0x2E
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002056, target byte: 0x00, byte in file: 0x09
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002057, target byte: 0x00, byte in file: 0xD3
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002058, target byte: 0x00, byte in file: 0x40
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002059, target byte: 0x00, byte in file: 0xF2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000205A, target byte: 0x00, byte in file: 0x12
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000205B, target byte: 0x00, byte in file: 0x32
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000205C, target byte: 0x00, byte in file: 0xDF
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000205D, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000205E, target byte: 0x00, byte in file: 0x98
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000205F, target byte: 0x00, byte in file: 0x15
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002060, target byte: 0x00, byte in file: 0xDF
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002061, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002062, target byte: 0x00, byte in file: 0x98
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002063, target byte: 0x00, byte in file: 0x05
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002065, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002066, target byte: 0x00, byte in file: 0xEC
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002067, target byte: 0x00, byte in file: 0xFA
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002068, target byte: 0x00, byte in file: 0xAF
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002069, target byte: 0x00, byte in file: 0xF3
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000206B, target byte: 0x00, byte in file: 0x80
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000206C, target byte: 0x00, byte in file: 0xDF
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000206D, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000206E, target byte: 0x00, byte in file: 0x90
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000206F, target byte: 0x00, byte in file: 0x05
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002071, target byte: 0x00, byte in file: 0xEB
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002072, target byte: 0x00, byte in file: 0x86
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002074, target byte: 0x00, byte in file: 0x80
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002075, target byte: 0x00, byte in file: 0x46
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002076, target byte: 0x00, byte in file: 0xD8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002077, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000207A, target byte: 0x00, byte in file: 0x03
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000207B, target byte: 0x00, byte in file: 0x21
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000207C, target byte: 0x00, byte in file: 0xB9
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000207D, target byte: 0x00, byte in file: 0x40
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000207E, target byte: 0x00, byte in file: 0x88
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000207F, target byte: 0x00, byte in file: 0x43
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002080, target byte: 0x00, byte in file: 0xED
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002081, target byte: 0x00, byte in file: 0xB2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002082, target byte: 0x00, byte in file: 0x15
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002083, target byte: 0x00, byte in file: 0xFA
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002084, target byte: 0x00, byte in file: 0x07
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002085, target byte: 0x00, byte in file: 0xF1
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002086, target byte: 0x00, byte in file: 0x08
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002087, target byte: 0x00, byte in file: 0x43
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002088, target byte: 0x00, byte in file: 0xC8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002089, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000208C, target byte: 0x00, byte in file: 0xBD
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000208D, target byte: 0x00, byte in file: 0xE8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000208E, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000208F, target byte: 0x00, byte in file: 0x81
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002090, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002091, target byte: 0x00, byte in file: 0xB5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002092, target byte: 0x00, byte in file: 0x04
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002094, target byte: 0x00, byte in file: 0x03
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002095, target byte: 0x00, byte in file: 0x21
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002096, target byte: 0x00, byte in file: 0x20
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x60002099, target byte: 0x00, byte in file: 0xB2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000209A, target byte: 0x00, byte in file: 0xFF
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000209B, target byte: 0x00, byte in file: 0xF7
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000209C, target byte: 0x00, byte in file: 0xD1
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000209D, target byte: 0x00, byte in file: 0xFF
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000209E, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x6000209F, target byte: 0x00, byte in file: 0xBD
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A0, target byte: 0x00, byte in file: 0xD0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A1, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A2, target byte: 0x00, byte in file: 0x84
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A3, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A4, target byte: 0x00, byte in file: 0x49
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A5, target byte: 0x00, byte in file: 0x08
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A6, target byte: 0x00, byte in file: 0x49
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A8, target byte: 0x00, byte in file: 0xC0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020A9, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020AA, target byte: 0x00, byte in file: 0x84
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020AB, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020AC, target byte: 0x00, byte in file: 0xD0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020AD, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020AE, target byte: 0x00, byte in file: 0x84
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020AF, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B0, target byte: 0x00, byte in file: 0xC9
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B1, target byte: 0x00, byte in file: 0x07
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B2, target byte: 0x00, byte in file: 0xFB
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B3, target byte: 0x00, byte in file: 0xD5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B4, target byte: 0x00, byte in file: 0x70
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B5, target byte: 0x00, byte in file: 0x47
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B6, target byte: 0x00, byte in file: 0xD0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B7, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B8, target byte: 0x00, byte in file: 0x80
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020B9, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020BA, target byte: 0x00, byte in file: 0x51
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020BB, target byte: 0x00, byte in file: 0xF0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020BC, target byte: 0x00, byte in file: 0x01
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020BD, target byte: 0x00, byte in file: 0x01
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020BE, target byte: 0x00, byte in file: 0xC0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020BF, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C0, target byte: 0x00, byte in file: 0x80
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C1, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C2, target byte: 0x00, byte in file: 0x70
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C3, target byte: 0x00, byte in file: 0x47
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C4, target byte: 0x00, byte in file: 0xD0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C5, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C6, target byte: 0x00, byte in file: 0x80
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C7, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C8, target byte: 0x00, byte in file: 0x49
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020C9, target byte: 0x00, byte in file: 0x08
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020CA, target byte: 0x00, byte in file: 0x49
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020CC, target byte: 0x00, byte in file: 0xC0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020CD, target byte: 0x00, byte in file: 0xF8
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020CE, target byte: 0x00, byte in file: 0x80
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020CF, target byte: 0x00, byte in file: 0x10
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D0, target byte: 0x00, byte in file: 0x70
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D1, target byte: 0x00, byte in file: 0x47
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D2, target byte: 0x00, byte in file: 0xC9
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D3, target byte: 0x00, byte in file: 0xB2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D4, target byte: 0x00, byte in file: 0x01
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D5, target byte: 0x00, byte in file: 0x64
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D6, target byte: 0x00, byte in file: 0x70
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D7, target byte: 0x00, byte in file: 0x47
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020D9, target byte: 0x00, byte in file: 0x68
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020DA, target byte: 0x00, byte in file: 0xC0
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020DB, target byte: 0x00, byte in file: 0xB2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020DC, target byte: 0x00, byte in file: 0x70
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020DD, target byte: 0x00, byte in file: 0x47
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020DE, target byte: 0x00, byte in file: 0x38
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020DF, target byte: 0x00, byte in file: 0xB5
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E0, target byte: 0x00, byte in file: 0x04
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E2, target byte: 0x00, byte in file: 0x0D
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E4, target byte: 0x00, byte in file: 0xED
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E5, target byte: 0x00, byte in file: 0xB2
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E6, target byte: 0x00, byte in file: 0x02
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E7, target byte: 0x00, byte in file: 0x2D
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E8, target byte: 0x00, byte in file: 0x02
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020E9, target byte: 0x00, byte in file: 0xDB
Wed Sep 19, 2018 22:23:53: Warning:
Verify error at address 0x600020EA, target byte: 0x00, byte in file: 0xED
Wed Sep 19, 2018 22:23:53: Warning: Too many verify errors, only the first 200 are displayed
Wed Sep 19, 2018 22:23:56: Warning: There were warnings during download, see Log Window
Wed Sep 19, 2018 22:23:56: Loaded debugee: C:\NXP\SDK_2.2_MCIM6ULL\boards\evkmcimx6ull\demo_apps\hello_world\iar\debug\hello_world.out
Wed Sep 19, 2018 22:23:56: Software reset was performed
Wed Sep 19, 2018 22:23:56: Target reset
Wed Sep 19, 2018 22:23:57: There was 1 warning during the initialization of the debugging session.

标记 (1)
0 项奖励
1 回复

591 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  I have some doubt regarding "Set boot mode to reserved mode (BMODE[1:0]=2'b11)".

Try using  Serial Downloader boot mode BMODE[1:0] = 01

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励