I.MX6UL Mic. Recording Problem!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6UL Mic. Recording Problem!!

584件の閲覧回数
dhanushvenugopa
Contributor I

Hi,

I am using IMX6ULevk board with wm8960 codec  but im facing problem of mic recording.when i give arecord command it records the audio without throwing any error but when i aplay the mic recorded wav file there is no output.

But when i aplay the demo wav files there is output through speakers.

so please can i know which part of driver/dts i need to cross check.

0 件の賞賛
返信
1 返信

512件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi  Dhanush

one can check registered audio devices using sect.7.1.2.4 Sound Card Information and some

alsa methods described in sect.7.4.3 attached Linux Manual.

Please try with Linux Binary Demo Files - i.MX 6UltraLite, i.MX 6ULL, i.MX 7Dual

May be useful some audio unit tests:

mxc_amix_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信