你好,I.MX6UL的 RM 中提到的音频功能MQS,
MQS is used to generate medium quality audio via a standard GPIO in the pinmux. The
user can connect stereo speakers or headphones to a power amplifier without an additional DAC chip.
但是网上的MQS的资料非常少。那么
1、MQS的输出波形是什么样式的?是不是类似SPWM?
2、MQS的输出功率是怎么样的?从上述英文来看只能接32Ω的耳机
3、MQS如果要外接大功率的喇叭,用哪种类型的功放芯片?A类?B类?D类都可以吗?
4、与功放的电路怎么接呢?是不是和普通的DAC输出的音频接法一样?
Hello jinsheng,
MQS是输出的PWM音频波,RIGHT和LEFT引脚直接接耳机,可以驱动并听到声音。如果需要放大的话,2个引脚各接一个NPN型三极管(接在B极,C极输出)就可以实现放大功能。
所以,你如果需要接放大器,你只需要把它们作为不带编码的数字信号,进行放大就可以了。接哪个类型的放大器,没有特别要求。
Have a great day,
TIC Weidong Sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------