Now I want to use PC as the HOST and i.mx6 as the device, but when I set it as follows, the driver appears on the i.mx6 board, but it cannot be recognized when using the OTG interface to connect。
and i found the driver has been installed successfully, but there is no response when the OTG is connected.
Hi chatty
one can check patches on
https://community.nxp.com/docs/DOC-336470
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear igorpadykov
This patch and link are not available. Could you please re-post them ?