I.MX6 NCM OTG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 NCM OTG

583 Views
1130692457
Contributor I

Now I want to use PC as the HOST and i.mx6 as the device, but when I set it as follows, the driver appears on the i.mx6 board, but it cannot be recognized when using the OTG interface to connect。

F9V[3[BJ}B8%QI4W{_F~JKQ.png

and i found  the driver has been installed successfully, but there is no response when the OTG is connected.

IMG_5123.PNG

Labels (2)
0 Kudos
2 Replies

461 Views
igorpadykov
NXP Employee
NXP Employee

Hi chatty

one can check patches on

carplay ncm 

https://community.nxp.com/docs/DOC-336470 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

461 Views
amit251291
Contributor IV

Dear igorpadykov

This patch and link are not available. Could you please re-post them ?

0 Kudos