I.MX6 NCM OTG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 NCM OTG

586件の閲覧回数
1130692457
Contributor I

Now I want to use PC as the HOST and i.mx6 as the device, but when I set it as follows, the driver appears on the i.mx6 board, but it cannot be recognized when using the OTG interface to connect。

F9V[3[BJ}B8%QI4W{_F~JKQ.png

and i found  the driver has been installed successfully, but there is no response when the OTG is connected.

IMG_5123.PNG

ラベル(2)
0 件の賞賛
2 返答(返信)

464件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chatty

one can check patches on

carplay ncm 

https://community.nxp.com/docs/DOC-336470 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

464件の閲覧回数
amit251291
Contributor IV

Dear igorpadykov

This patch and link are not available. Could you please re-post them ?

0 件の賞賛