I.MX6 DualLite with NFC PN544 on imx-3.14.28-1.0.1_patch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 DualLite with NFC PN544 on imx-3.14.28-1.0.1_patch

1,385 Views
kunyichen
Contributor IV

Hi

     I work on IMX6DL SABRESD with NXP PN544,

BSP use Yocto L3.14.28-1.0.1_patch release

 

currently want know how to testing PN544 with tag,

I use the following step, but always can not get a correct result.

Would have anyone give something tips?

 

 

imx6dl login: root

root@imx6dl :~# /etc/init.d/neard stop

Stopping Linux NFC daemon

Terminated

root@imx6dl:~# cd /usr/lib/neard/

 

root@imx6dl:/usr/lib/neard# ./neard -d -n &

[1] 975

root@imx6dl:/usr/lib/neard# neard[975]: NEAR daemon version 0.14

neard[975]: src/dbus.c:__near_dbus_init()

neard[975]: src/netlink.c:__near_netlink_init()

neard[975]: src/netlink.c:nl_get_multicast_id()

neard[975]: src/netlink.c:__nl_send_msg()

neard[975]: src/netlink.c:family_handler()

neard[975]: src/netlink.c:ack_handler()

neard[975]: src/netlink.c:nl_get_multicast_id() multicast id 7

neard[975]: src/agent.c:__near_agent_init()

neard[975]: src/tag.c:__near_tag_init()

neard[975]: src/device.c:__near_device_init()

neard[975]: src/adapter.c:__near_adapter_init()

neard[975]: src/ndef.c:__near_ndef_init()

neard[975]: src/manager.c:__near_manager_init()

neard[975]: src/manager.c:__near_manager_init() connection 0x492e58

neard[975]: src/netlink.c:__near_netlink_get_adapters()

neard[975]: src/netlink.c:__nl_send_msg()

neard[975]: src/netlink.c:get_devices_handler()

neard[975]: src/manager.c:__near_manager_adapter_add() idx 0

neard[975]: src/adapter.c:__near_adapter_create() Powered 0

neard[975]: src/adapter.c:__near_adapter_add() /org/neard/nfc0

neard[975]: src/adapter.c:__near_adapter_add() connection 0x492e58

neard[975]: src/netlink.c:__finish_handler()

neard[975]: src/bluetooth.c:__near_bluetooth_init()

neard[975]: src/plugin.c:__near_plugin_init()

neard[975]: plugins/p2p.c:p2p_init()

neard[975]: plugins/phdc.c:phdc_init()

neard[975]: plugins/p2p.c:near_p2p_register() driver 0x3f68c name NPP service com.android.npp

neard[975]: plugins/p2p.c:near_p2p_register() driver 0x3f6b4 name SNEP service urn:nfc:sn:snep

neard[975]: plugins/p2p.c:near_p2p_register() driver 0x3f6dc name VALIDATION_SNEP service urn:nfc:xsn:nfc-forum.org:snep-validation

neard[975]: plugins/llcp-validation.c:llcp_validation_init()

neard[975]: plugins/p2p.c:near_p2p_register() driver 0x3f704 name VALIDATION_LLCP_CL service urn:nfc:sn:cl-echo

neard[975]: plugins/p2p.c:near_p2p_register() driver 0x3f72c name VALIDATION_LLCP_CO service urn:nfc:sn:co-echo

neard[975]: plugins/p2p.c:near_p2p_register() driver 0x3f754 name Handover service urn:nfc:sn:handover

neard[975]: src/device.c:near_device_driver_register()

neard[975]: src/adapter.c:adapter_listen() /org/neard/nfc0

neard[975]: plugins/p2p.c:p2p_bind()

neard[975]: plugins/p2p.c:__p2p_bind() Binding Handover

neard[975]: plugins/p2p.c:p2p_bind()

neard[975]: plugins/p2p.c:__p2p_bind() Binding VALIDATION_LLCP_CO

neard[975]: plugins/p2p.c:p2p_bind()

neard[975]: plugins/p2p.c:__p2p_bind() Binding VALIDATION_LLCP_CL

neard[975]: plugins/p2p.c:p2p_bind()

neard[975]: plugins/p2p.c:__p2p_bind() Binding VALIDATION_SNEP

neard[975]: plugins/p2p.c:p2p_bind()

neard[975]: plugins/p2p.c:__p2p_bind() Binding SNEP

neard[975]: plugins/p2p.c:p2p_bind()

neard[975]: plugins/p2p.c:__p2p_bind() Binding NPP

neard[975]: plugins/nfctype4.c:nfctype4_init()

neard[975]: src/tag.c:near_tag_driver_register()

neard[975]: src/tag.c:near_tag_driver_register()

neard[975]: plugins/nfctype3.c:nfctype3_init()

neard[975]: src/tag.c:near_tag_driver_register()

neard[975]: plugins/nfctype2.c:nfctype2_init()

neard[975]: src/tag.c:near_tag_driver_register()

neard[975]: plugins/nfctype1.c:nfctype1_init()

neard[975]: src/tag.c:near_tag_driver_register()

neard[975]: src/agent.c:register_handover_agent() conn 0x492e58

neard[975]: src/agent.c:handover_register() sender :1.0 path /net/connman/neard_handover_agent carrier wifi

neard[975]: src/agent.c:create_handover_agent() handover agent registered

neard[975]: src/adapter.c:append_protocols() protocols 0x7e

 

root@imx6dl:/usr/lib/neard# ./test-adapter list

neard[975]: src/adapter.c:append_protocols() protocols 0x7e

[ /org/neard/nfc0 ]

    Protocols = [ Felica MIFARE Jewel ISO-DEP NFC-DEP ]

    Mode = Idle

    Polling = false

    Powered = false

root@imx6dl:/usr/lib/neard# ./test-adapter powered nfc0 on

neard[975]: src/adapter.c:append_protocols() protocols 0x7e

neard[975]: src/netlink.c:__near_pn544_i2c: pn544_hci_i2c_enable

netlink_adapter_enable()

neard[975]: src/netlink.c:__nl_send_msg()

hci: hci_dev_version: SOFTWARE INFO:

hci: hci_dev_version: RomLib         : 11

hci: hci_dev_version: Patch          : 1

hci: hci_dev_version: FlashLib Major : 1

hci: hci_dev_version: FlashLib Minor : 26

hci: hci_dev_version: HARDWARE INFO:

hci: hci_dev_version: Derivative     : 3

hci: hci_dev_version: HW Version     : 2

hci: hci_dev_version: #MPW           : 0

hci: hci_dev_version: Software       : 0

hci: hci_dev_version: BSID Version   : 3

neard[975]: src/netlink.c:ack_handler()

neard[975]: src/netlink.c:no_seq_check()

neard[975]: src/netlink.c:nfc_netlink_event() event 0x16

root@imx6dl:/usr/lib/neard# ./test-adapter poll nfc0 on Initator

neard[975]: src/adapter.c:append_protocols() protocols 0x7e

neard[975]: src/adapter.c:start_ppn544: HCI NFC driver for PN544: pn544_hci_start_poll protocols 0x7e 0x0

oll_loop() conn 0x492e58

neard[975]: src/adapter.c:start_poll_loop() Mode Initator

neard[975]: src/adapter.c:adapter_start_poll() Poll mode 0x1

neard[975]: src/netlink.c:__near_netlink_start_poll() IM protos 0x7e TM protos 0x0

neard[975]: src/netlink.c:__nl_send_msg()

neard[975]: src/netlink.c:ack_handler()

###

### at step I put some NDEF card to close PN544 reader

### then run the below step

root@imx6dl:/usr/lib/neard# ./test-tag list                   

neard[975]: src/adapter.c:append_protocols() protocols 0x7e

root@imx6dl:/usr/lib/neard# ./test-tag dump

neard[975]: src/adapter.c:append_protocols() protocols 0x7e

root@imx6dl:/usr/lib/neard# ./test-adapter list

neard[975]: src/adapter.c:append_protocols() protocols 0x7e

[ /org/neard/nfc0 ]

    Protocols = [ Felica MIFARE Jewel ISO-DEP NFC-DEP ]

    Mode = Idle

    Polling = true

    Powered = true

Original Attachment has been moved to: dmesg_nfc.txt.zip

Labels (4)
4 Replies

796 Views
igorpadykov
NXP Employee
NXP Employee

Hi KunYi

I am not aware of i.MX6 BPSs nfc support, but it may be added following next links

linux-2.6-imx.git - Freescale i.MX Linux Tree

AN11697  Linux Software Stack Integration Guidelines

http://www.nxp.com/documents/application_note/AN11697.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

796 Views
kunyichen
Contributor IV

Hi Igor,

    First thank for your reply

    Currently the BSP should support PN544, 

    Yocto/L3.14.28 support "neard" project and linux mainstream support nfc into net interface now

    You can review my attached file and steps, the PN544 I2C/HCI driver has built-in into kernel

    But I'll try AN1167 note! but I know mainstream has accept neard project and integration into kernel tree

0 Kudos
Reply

796 Views
kunyichen
Contributor IV

okay, I have been testing AN1167, still failed

I think the appnote AN1167 should be just support PN7120, due to the library just support NCI interface, not support ETSI/HCI

0 Kudos
Reply

796 Views
igorpadykov
NXP Employee
NXP Employee

unfortunately I am not aware of PN7120 drivers for i.MX6, in general

NXP has service for porting drivers : NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

~igor