iMX6Q : How to use the /WDOG1 signal before the uboot is booting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q : How to use the /WDOG1 signal before the uboot is booting

Jump to solution
746 Views
koichisakagami
Contributor II

Dear community,
We have been developing our product with iMX6Q.

In figure 8-2 USB Boot Flow of IMX6DQRM Rev. 3,
it said ARM core will reset if no any activity within 90 seconds when WDOG_ENABLE=1.

[Question]
    Then, is the /WDOG1 signal  outputed to iMX6 I/O pin ?
    (DISP0_DAT8 pad or GPIO_9 pad or SD1_DATA2 pad)

  

    I  want to use the /WDOG1 signal for being detected external device .

Best Regards,
    Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
546 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Software (internal) reset is produced by the  internal serial  boot ROM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
547 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Software (internal) reset is produced by the  internal serial  boot ROM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply