don't such document besides the machine learning user guide I sent to you
OVXLIB and OpenVX driver integrated with NXP
GPU driver package
− Provides low-level calls to NPU hardware
− Implemented as OpenCL kernels for GPUs of i.MX
8M, 8M Nano and 8QuadXPlus
− i.MX 8QuadMax OpenVX hardware extension
accelerates OpenVX instructions and has a significant
performance advantage over running on shader core
for imx8mp:
openvx hardware extension is available in the i.MX8MP NPU, which means that OpenVX hardware acceleration is performed on the NPU, not on the GPU
so for gpu or npu demo module, you can find the test demo in the bsp , for imx8mp demo, which is still internal use, I couldn't share with outside customer
refer to the application note as below:
https://www.nxp.com/docs/en/application-note/AN12060.pdf
the demo code you can find:
https://github.com/NXPmicro/gtec-demo-framework/tree/master/DemoApps
Hi, Joanxie
Thank You tell me about ISP & OpenVX information, But it's not My need.
I want to know "HOW to use ovxlib on NPU/GPU" , or any related document .
Example 1 : enable inference engine
VSI_NN_LOG_LEVEL=0 {bin} -m {model} -t 1 -i {Image} -l {label} -a 1 -v 0 -c 100
Example 2 : Using Ovxlib library
vsi_nn_VerifyGraph, vsi_nn_AddNode etc....
Or... How to get VX/vx_ext_program.h
like this link :OpenVX Vision Image Extension API Introduction - Basic API
Thank your help so much
Hi, joanxie
thank your help , this document taught me some operations with NPU/GPU (at Appendix A &B),
but it's not about "ovxlib" or "VSI_NN_LOG_LEVEL" using way...
I appreciate your help very much.
don't such document besides the machine learning user guide I sent to you
OVXLIB and OpenVX driver integrated with NXP
GPU driver package
− Provides low-level calls to NPU hardware
− Implemented as OpenCL kernels for GPUs of i.MX
8M, 8M Nano and 8QuadXPlus
− i.MX 8QuadMax OpenVX hardware extension
accelerates OpenVX instructions and has a significant
performance advantage over running on shader core
for imx8mp:
openvx hardware extension is available in the i.MX8MP NPU, which means that OpenVX hardware acceleration is performed on the NPU, not on the GPU
so for gpu or npu demo module, you can find the test demo in the bsp , for imx8mp demo, which is still internal use, I couldn't share with outside customer
I would like to use NPU of imx8mp. At the moment I am on a 5.10 mainline kernel, but it seems that I need parts of NXP kernel for accessing the NPU. From the other post it seems like that gpu-viv is needed (and its part of devicetree). Is this right - even if computation is not done on GPU but NPU? At least I don't find a dedicated NPU kernel driver. Can you advise?