Hi,
I am using one USB OTG port as device. I can confirm that the OTG port is working when using Mfgtool for flashing images.
When building the kernel the USB gadget can be configured to only Gadget mass storage and UTP.
After flashing the images and booting, I want the same port to be used as either gadget serial or gadget HID. But we configured the USB as gadget mass storage. If I give other option such as CONFIG_GADGET_SERIAL or HID I am unable to flash the images.
What is the right option to make it as GADGET MASS STORAGE and GADGET SERIAL?
I tried building the kernel and modules in separate builds, but when I try to do modprobe g_serial
modprobe g_serial
modprobe: can't load module libcomposite (kernel/drivers/usb/gadget/g_serial.ko): invalid module format
I am getting this error.
Hi chandra
please try usb hid examples in imx-test (../mxc_usb_test) and description
in attached Linux Manual Chapter 39 CHIPIDEA USB Driver
imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
I am able to run modeprobe g_serial and able to see the serial device in /dev folder.
I want to change the baud rate of the same, if I give the below commands it is throwing error
stty -F /dev/ttyGS0 921600
stty: /dev/ttyGS0: cannot perform all requested operations
Is there any way to change the baudrate. Here the default baudrate is 9600. I want to operate at 921600 bps.
Hi igorpadykov
Is there any way to check whether the g_serial device is connected or not??