Hi All,
I'm trying to update the spa_supplicant package included in ltib, because I see that it's an old package 0.5.9 and now the release is 2.0.
Could someone help me?
I try to put the spa_supplicant-2.0.tar.gz package in /opt/freescale/pkgs and change the spec to point to it, but ltib crash in compilation.
Thanks a lot for the help
Dario
已解决! 转到解答。
Found the solution: I had to add 'cd wpa_supplicant' in wpa_supplicant.spec file here:
%Build
#aggiunto per v2.0
cd wpa_supplicant
and
%Install
#aggiunto per v2.0
cd wpa_supplicant
This is because the structure of the new package is different from the old one.
Regards
Dario
Found the solution: I had to add 'cd wpa_supplicant' in wpa_supplicant.spec file here:
%Build
#aggiunto per v2.0
cd wpa_supplicant
and
%Install
#aggiunto per v2.0
cd wpa_supplicant
This is because the structure of the new package is different from the old one.
Regards
Dario
Most of the times, when updating a package it is not enough to just change the version. You can either jump to the LTIB console, follow the spec tasks manually, and see if things go well OR try Yocto, the package is already there as seen in the following find's log
./meta-openembedded/meta-systemd/oe-core/recipes-connectivity/wpa-supplicant
./meta-openembedded/meta-systemd/oe-core/recipes-connectivity/wpa-supplicant/wpa-supplicant_2.0.bbappend
./poky/meta/recipes-connectivity/wpa-supplicant
./poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant-2.0.inc
./poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant_2.0.bb
./poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant
./poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant/wpa_supplicant.conf
./poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant/wpa-supplicant.sh
./poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant/99_wpa_supplicant
./poky/meta/recipes-connectivity/wpa-supplicant/wpa-supplicant/wpa_supplicant.conf-sane
b42214@vfae-server:~/fsl/yocto/fsl-community-bsp-dylan/sources$
Leo
A bit late but to jump to the console, just run ./ltib -m shell assuming that you have prepare (./ltib -m prep), move to the corresponding BUILD folder (rpm/BUILD/wpa...) then follow the tasks manually ( For example, ./configure && make & make install). Nice that you found a solution. Leo