How to underclock an iMX6 Quad Sabre Lite board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to underclock an iMX6 Quad Sabre Lite board?

Jump to solution
1,584 Views
blevefrancesco
Contributor I

I need to underclock an iMX6 Quad Sabre Lite board down to 800 MHz.

At the moment on this board I'm running Yocto Linux and Android 5.1.1.

For Yocto Linux I read on this forum that is possible to accomplish it modifying the BSP, before building the image, but I didn't find any suggestion on how to do it.

I would be glad if someone could explain me in which way I should modify the BSP.

For Android 5.1.1 instead I'm running a ready made image, built by Boundary Devices (for Android 5.1.1 there is no source code provided).

Could be possible to underclock the board even with a ready made image?

Otherwise I would have to downgrade to Android 5.0 for which they provide the source code and try to underclock that one.

Also in this case, any suggestion on how to do it?

Thanks!

0 Kudos
Reply
1 Solution
1,295 Views
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

one can try to change cpu frequency working points as described in

attached Linux Manual sect.24.1.2 Source Code Structure

Best regards

igor

View solution in original post

0 Kudos
Reply
2 Replies
1,296 Views
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

one can try to change cpu frequency working points as described in

attached Linux Manual sect.24.1.2 Source Code Structure

Best regards

igor

0 Kudos
Reply
1,295 Views
blevefrancesco
Contributor I

Thank you!

I found also this useful guide on the internet that could help people with the same issue:

https://software.intel.com/sites/default/files/comment/1716807/how-to-change-frequency-on-linux-pub....

0 Kudos
Reply