How to underclock an iMX6 Quad Sabre Lite board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to underclock an iMX6 Quad Sabre Lite board?

ソリューションへジャンプ
1,344件の閲覧回数
blevefrancesco
Contributor I

I need to underclock an iMX6 Quad Sabre Lite board down to 800 MHz.

At the moment on this board I'm running Yocto Linux and Android 5.1.1.

For Yocto Linux I read on this forum that is possible to accomplish it modifying the BSP, before building the image, but I didn't find any suggestion on how to do it.

I would be glad if someone could explain me in which way I should modify the BSP.

For Android 5.1.1 instead I'm running a ready made image, built by Boundary Devices (for Android 5.1.1 there is no source code provided).

Could be possible to underclock the board even with a ready made image?

Otherwise I would have to downgrade to Android 5.0 for which they provide the source code and try to underclock that one.

Also in this case, any suggestion on how to do it?

Thanks!

ラベル(6)
0 件の賞賛
1 解決策
1,055件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

one can try to change cpu frequency working points as described in

attached Linux Manual sect.24.1.2 Source Code Structure

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,056件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

one can try to change cpu frequency working points as described in

attached Linux Manual sect.24.1.2 Source Code Structure

Best regards

igor

0 件の賞賛
1,055件の閲覧回数
blevefrancesco
Contributor I

Thank you!

I found also this useful guide on the internet that could help people with the same issue:

https://software.intel.com/sites/default/files/comment/1716807/how-to-change-frequency-on-linux-pub....

0 件の賞賛