We use SN65DSI83-Q1 to transform MIPI DSI signal to LVDS.
SN65DSI83-Q1’s initization need "After power is applied and stable, all DSI input lanes including DSI CLK(DA × P/N) must be driven to LP11 state."
How can I set dsi mipi lanes to LP11 status On i.mx serie(imx8 imx6)
Thanks.
As an example for the i.MX6 series processors, please refer to the Chapter 41 "MIPI DSI Host Controller (MIPI_DSI)", especially, to the Sections 41.6.8 "Video Mode Configuration (MIPI_DSI_VID_MODE_CFG)" and below of the i.MX6Dual/Quad Reference Manual document, available on the processor's Documentation web page:
Have a great day,
Artur