How to set dsi mipi lanes to LP11 status

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set dsi mipi lanes to LP11 status

3,169 Views
xinchuan
Contributor III

We use SN65DSI83-Q1 to transform MIPI DSI signal to LVDS.

SN65DSI83-Q1’s initization need "After power is applied and stable, all DSI input lanes including DSI CLK(DA × P/N) must be driven to LP11 state."

How can I set dsi mipi lanes to LP11 status On i.mx serie(imx8 imx6)

Thanks.

Labels (2)
5 Replies

406 Views
illy777
Contributor III

Hello I'm facing the same issue and could not find an appropiate answer... Does someone have a solution?

0 Kudos
Reply

2,317 Views
art
NXP Employee
NXP Employee

As an example for the i.MX6 series processors, please refer to the Chapter 41 "MIPI DSI Host Controller (MIPI_DSI)", especially, to the Sections 41.6.8 "Video Mode Configuration (MIPI_DSI_VID_MODE_CFG)" and below of the i.MX6Dual/Quad Reference Manual document, available on the processor's Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...


Have a great day,
Artur

0 Kudos
Reply

2,317 Views
guido_gunther
Contributor II

Artur Petukhov schrieb:

As an example for the i.MX6 series processors, please refer to the Chapter 41 "MIPI DSI Host Controller

How would that work on the i.MX8M?

2,317 Views
sbertrand
Contributor III

Hi,

I am facing a similar question for the TC358767 DSI to DisplayPort bridge.

Did you figure out something ?

Regards,
Stan

367 Views
illy777
Contributor III

Are there any updated?

0 Kudos
Reply