Hi,
I am using imx8mq and 4.9.51 Linux distribution. I have connected processor's SAI1 to analog devices'ADAU1361 codec.(I2S interface)
My codec is working with external oscillator(12.288Mhz)MCLK. But i need to change clock source form external to internal.(i.e from processor's mclk pin).
The MCLK is generated from processor when i play audio.
Actually i need continues MCLK.
My query is
1) How to set continues mclk on in processor side?
Let me know if you need further information.
Thanks & regards,
Parth
Hi Igor,
Thanks for the reference.
This take lots of time to learn and We have little urgency to do this.
So,Can you please point out the exact function to set a mclk frequency and where to call?
Thanks & regards,
Parth
Hi Parth
I am afraid there are no ready patches for that.
If you have some project requiring this feature, suggest to proceed with
Professional Services to develop solution:
As simple workaround one can consider CCM_CLKO1,2 for outputting
continuous clock.
Best regards
igor
Hi Parth
unfortunately there is no such option in dts file for such case, seems
driver modifications are needed. One can try to analyze driver sources in
linux/sound/soc/fsl/fsl_sai.c
fsl_sai.c\fsl\soc\sound - linux-imx - i.MX Linux kernel
use alsa tutorial:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------