I am a little confused on what the NAND_row_address_bytes[1:0] setting actually means. We are working with a Cypress S34ML08G1 (full PN S34ML08G101BHI003). Attached is the NAND boot cycles for the memory that suggests that there are 3 Row Addresses and 2 Column Addresses for 5 Memory Addresses total.
According to the wording of the i.MX6 TRM and the table that is attached, the setting of BOOT_CFG1[1:0] should be 0b00 which corresponds to 3 row addresses.
I am confused by two other pieces of data.
Which value should I set BOOT_CFG1[1:0] to with a Spansion memory with 3 row addresses, but 5 total memory addresses?
Thank you,
Adam
Hi Adam
description in RM is correct so BOOT_CFG1[1:0] should be 0b00.
Mentioned link has correct last answer.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------