How to save video stream into multiple files without stop gstreamer pipeline?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to save video stream into multiple files without stop gstreamer pipeline?

2,862 Views
RobbieJiang
Contributor IV

Hi,

I'm using a gstreamer pipeline to save encoded video stream into files on iMX515/Linux-2.6.31 platform.

The pipeline is as follows:

mfw_v4lsrc -> mfw_vpuencoder -> avimux -> filesink location=xxx

However, I would like to change the file name ( i.e, the "location" propoerty of filesink element )

every 10 minutes( e.g, change the file name to the current time ).

AndI don't want to stop the pipeline before changing the location property.

With gstreamer-1.2 or higher version, it's possible to do this with gst_pad_set_block(),

that is, blocking the source pad of avimux first, set filesink's state to NULL, change the location property,

set filesink's state to ready, and unblock avimux's source pad. ( Or something like that, I'm not quite sure.)

But the gstreamer library comes with imx515 BSP is gstreamer-0.10.x.

I am not sure if this method can make any sense with our work platform.

Is there anyone who has done this successfully?

Or is there another method to try?

Robbie

Labels (2)
0 Kudos
Reply
0 Replies