How to porting from iMX6D to iMX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to porting from iMX6D to iMX6DL

1,554件の閲覧回数
yuzheng
Contributor I

we are developing the BSP of iMX6D : MCIMX6D5EYM10ad SBOX1519, and we can boot the u-boot and kernel in our board now;

but we just change the CPU of our board, and change it to iMX6DL : MCIMX6U5EVM10AC XAC1551, other parts keep no change.

could you tell me how to porting uboot and kernel from iMX6D to iMX6DL?

is there a user guide? or some practices?

thanks in advance!

ラベル(3)
0 件の賞賛
返信
6 返答(返信)

1,333件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Could you tell me which BSP are you using?

Have a nice day

Rita

0 件の賞賛
返信

1,333件の閲覧回数
yuzheng
Contributor I

we are using the Q7 board of Advantech, and get the initial BSP from them;

the kernel version is 4.1-r0, the u-boot version is v2016.07+gitAUTOINC+ae973bc45d-r0;

and use Yokto to compile the BSP;

i don't find the exact version of this BSP, could you tell me how to look at the version?

thanks

0 件の賞賛
返信

1,333件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Here you are using the board from Advantech, details design and porting you can contact them.  In our website there're i.MX_BSP_Porting_Guide.pdf  and Freescale_Yocto_Project_User's_Guide.pdfdocument for custom. You can refer to . 

Hope this can help you
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,333件の閲覧回数
aravinthkumarja
Senior Contributor II

Which BSP you are using?

0 件の賞賛
返信

1,333件の閲覧回数
yuzheng
Contributor I

we are using the Q7 board of Advantech, and get the initial BSP from them;

the kernel version is 4.1-r0, the u-boot version is v2016.07+gitAUTOINC+ae973bc45d-r0;

and use Yokto to compile the BSP;

0 件の賞賛
返信

1,333件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi yn zheng,

You need to get iMX6DL environment setup from Advantech. And then you can able to build for iMX6DL. 

For your reference:

Porting iMX6D to iMX6DL

0 件の賞賛
返信