How to port DSI on IMX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to port DSI on IMX7D

926 Views
864535720
Contributor II

hi:

   How to port DSI on IMX7D?

   Can IMX7D not support both LCD and DSI?

Labels (1)
0 Kudos
Reply
2 Replies

793 Views
igorpadykov
NXP Employee
NXP Employee

Hi 其东

in general i.IMX7D can not support both parallel LCD and DSI as

both use one eLCDIF module. Porting will be performing specific for panel

configuration commands, setting timings using sect.6.4 MIPI DSI attached Linux Manual

and example of TRULY-WVGA-TFT3P5581E display, which is supported by default

(reference can be found in arch/arm/boot/dts/imx7d-sdb-mipi-dsi.dts)

linux-imx.git - i.MX Linux Kernel 

static struct fb_videomode truly_lcd_modedb[] = {
{
"TRUULY-WVGA", 50, 480, 854, 41042,
40, 60,
3, 3,
8, 4,
FB_SYNC_OE_LOW_ACT,
FB_VMODE_NONINTERLACED,
0,
},
};

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

793 Views
864535720
Contributor II

Hello, I don't know how to build the device tree. I tried to port the content from imx7d-sdb-mipi-dsi.dts, but without success, can you give a transplanted document and sample?

0 Kudos
Reply