Hi
I just managed to bitbake the fsl-image-x11 image for the IMX6Q Sabre Board, and i'm now trying to use gstreamer to stream a webcam over the network.
It appears x264enc is not installed, so i tried to do it.
I tried multiple solutions found on the community forum ( Re: How to include x264enc on yocto and Task #9 - How to add bad/ugly ) but i'm getting the same error, for both solutions when using bitbake.
ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
fatal: reference is not a tree: 585324fee380109acd9986388f857f413a60b896
ERROR: Logfile of failure stored in: /media/philippe/data/fsl-release-bsp/build-x11/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/x264/r2265+gitAUTOINC+585324fee3-r0/temp/log.do_unpack.9681
Log data follows:
...
| DEBUG: Python function base_do_unpack finished
| DEBUG: Python function do_unpack finished
| ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
| fatal: reference is not a tree: 585324fee380109acd9986388f857f413a60b896
|
ERROR: Task 4108 (/media/philippe/data/fsl-release-bsp/sources/poky/meta/recipes-multimedia/x264/x264_git.bb, do_unpack) failed with exit code '1'
Does anyone have an idea about this issue?
Thanks in advance.
已解决! 转到解答。
Seems like the hash was incorrect, since they did tree maintenance.
Here's the one you should put in x264_git.bb : bfed708c5358a2b4ef65923fb0683cefa9184e6f