Hi All,
I am working on IMX8QM-MEK with Android 9 Automotive. These are the observation I found with default Power Management behavior.
These are the observation
1, No interrupt triggered for Wake-up
mek_8q:/ $ cat /sys/power/pm_wakeup_irq
cat: /sys/power/pm_wakeup_irq: No data available
2, Only timer expires concept is integrate
system/core/libsuspend/autosuspend.c
int autosuspend_force_suspend(int timeout_ms) {
int ret;ret = autosuspend_init();
if (ret) {
return ret;
}return autosuspend_ops->force_suspend(timeout_ms);
}
3, Deep sleep due to disable the following
source/vendor/nxp-opensource/kernel_imx/kernel/power
disable_nonboot_cpus
oom_killer_disable
arch_suspend_disable_irqs
4, Wake up is done due to enable the system clock and peripherals
source/vendor/nxp-opensource/kernel_imx/kernel/power
enable_nonboot_cpus
oom_killer_enable
arch_suspend_enable_irqs
I needs to implement enable clocks from m4 MCU.
Is there any per-defined API for enable clocks from M4 MCU ?
Thanks & Regards,
Vinoth S,
Solution here,
IMX8QM-MEK Power Management difference between Linux and Android
Regards,
VinothS.
Hi Vinoth
opposite to previous i.MX products, for i.MX8(X) there is no CCM Chapter in
Reference Manual and no direct access to CCM registers (and PLLs) are allowed.
All access is performed using Linux SCFW APIs :
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------