How to enable WIFI driver for AR6103 (SDIO) on IMX53 ARD board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable WIFI driver for AR6103 (SDIO) on IMX53 ARD board?

7,026 Views
Swamy
Contributor III

Hi All,

Please help me to enable WIFI driver AR6103 SDIO interface with Android for IMX53 ARD board.

Please suggest.

Regards,

Swamy

Labels (1)
0 Kudos
Reply
20 Replies

2,907 Views
Swamy
Contributor III

Sorry for troubling you, i am not sure how we make the environment clean of repo, please explain

Regards

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

It belongs compile error, please make sure you didn't back up 298's code in your project because there is also a ar6000.ko's compile task there. Use a clean environment please. this compile error is easy to solve.Please don't repeat the same error again and again here. 

how to solve this compile error can google it,

refer to 

http://forum.cyanogenmod.com/topic/35279-need-help-build-error/

http://groups.google.com/group/android-building/browse_thread/thread/f52c8d58af7420ad

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

I tried "mm" command, everything was OK. after that i used make clean and make distclean and followed by make..but still I am getting the same error!

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

Can you try to run "mm" command in system/wlan/atheros to see if OK? if OK, you maybe need a clean environment to try.

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

I am getting this error when I include RC.563...Please let me know where I need to make changes?

Regards,

Swamy

build/core/main.mk:303: implicitly installing apns-conf_sdk.xml
build/core/base_rules.mk:479: warning: overriding commands for target `out/target/product/imx53_ard/system/wifi/ath6k/AR6003/hw2.1.1/bdata.SD31.bin'
build/core/base_rules.mk:479: warning: ignoring old commands for target `out/target/product/imx53_ard/system/wifi/ath6k/AR6003/hw2.1.1/bdata.SD31.bin'
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/Android.mk:107: warning: overriding commands for target `/home/android/myandroid/system/wlan/atheros/AR6kSDK.build_3.1_RC.563/dummy'
system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/Android.mk:107: warning: ignoring old commands for target `/home/android/myandroid/system/wlan/atheros/AR6kSDK.build_3.1_RC.563/dummy'
system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/Android.mk:113: warning: overriding commands for target `system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/os/linux/ar6000.ko'
system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/Android.mk:113: warning: ignoring old commands for target `system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/os/linux/ar6000.ko'
build/core/base_rules.mk:162: *** system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host: MODULE.TARGET.ETC.ar6000.ko already defined by system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host.  Stop.

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

you should try to solve the compile error when using AR6kSDK.build_3.1_RC.563. Don't use 298's driver only including hw2.1.1. 298's driver don't support hw2.1.1.

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

Also i tried

bash-3.2# insmod ar6000.ko

I am getting this message....

bash-3.2# AR6000: Unsupported configuration opcode: 3
AR6000: SDIO bus operation failed! MMC stack returned : -84
Unable to read RX_LOOKAHEAD_VALID register
Unable to read Target Version from the device

Regards,

Swamy

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

Hi Jianzheng Zhou,

I included /system/wifi/ath6k/ AR6003/ hw2.1.1 and built. Now I am getting this error, when I tried to connect the WIFI.

I did not include myandroid\system\wlan\atheros\AR6kSDK.build_3.1_RC.563 as it was giving compilation error.

Please suggest.

Regards,

Swamy

AR6000: Unsupported configuration opcode: 3
AR6000: Unsupported configuration opcode: 3
HIF Interrupt processing is SYNC ONLY
AR6000: Unsupported configuration opcode: 7
AR6000: Unsupported configuration opcode: 5


In aggr_init..going out of aggr_init..status OK
Unknown firmware revision: 805307778
ar6000_avail: ar6000_sysfs_bmi_get_config failed

after 1mins I got this message,

init: untracked pid 2501 exited
aggr_module_destroy(): aggr = dffe0000
out aggr_module_destroy

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

Yes, Pls have a try. 

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

Sorry, I have one more question,

In my ARD board I am using following atheros kit

In the path myandroid\system\wlan\atheros\AR6kSDK.3.0_RC.298

But when I referred SMD, it was having myandroid\system\wlan\atheros\AR6kSDK.build_3.1_RC.563

which is a different version. Shall I copy this too to my system\wlan\atheros? and look for the path myandroid\system\wlan\atheros\AR6kSDK.build_3.1_RC.563 under Boardconfig.mk?

For your information when I checked in SMD board, the SDIO Atheros 6103 works fine..

Regards,

Swamy

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

1)In our newer software release there is this file. This file can be omitted. Not using it in fact.

2)No need to change code. you just need to add a hw2.1.1 folder alike hw2.0 in /system/wifi/ath6k/ AR6003 folder. The driver will auto search /system/wifi/ath6k/ AR6003/ hw2.1.1 folder if it detect it is a AR6103 wifi module.

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

Thanks for the reply.

1)

I could find all the mentioned files, but I was not able to find endpointping.bin, may i know where can i get it?

2)

Then, in the code please tell me which file does actually looks for this path hw2.1.1, so that i modify from hw2.0 to hw2.1.1.

Regards,

Swamy

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

Yes, you can use our newer software version--10.3.2. Or you can manually copy hw2.1.1 firmware from SMD. ensure all the following firmware are included in hw2.1.1 folder:

athtcmd_ram.bin athwlan_mobile.bin athwlan_tablet.bin data.patch.hw3_0.bin endpointping.bin
athwlan.bin athwlan_router.bin bdata.SD31.bin device.bin otp.bin

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

It is not available in the path you have mentioned. I could only see hw2.0 there. Please tell me which file does actually looks for this path?

Also, i have this hw2.1.1 firmware in SMD, can i copy that to here?

Please suggest.

Regards,

Swamy

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

AR6000: SDIO bus operation failed! MMC stack returned : -84

Wifi driver is loaded fail. Can you see if there is hw2.1.1's firmware in /system/wifi/ath6k/ AR6003/hw2.1.1/?

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

Hello Jianzheng Zhou,

Please suggest..

Some more log information...

# AR6000: Unsupported configuration opcode: 3
AR6000: SDIO bus operation failed! MMC stack returned : -84
Unable to read RX_LOOKAHEAD_VALID register
Unable to read Target Version from the device
init: untracked pid 2609 exited

0 Kudos
Reply

2,911 Views
Swamy
Contributor III

bash-3.2# AR6000: SDIO bus operation failed! MMC stack returned : -84
Unable to decrement the command credit count register
Unable to write to the device

Under logcat....

I/ActivityManager( 2160): Displayed com.android.settings/.WirelessSettings: +416ms
E/WifiHW  ( 2160): Unable to open connection to supplicant on "/data/system/wpa_supplicant/eth1": No such file or directory
I//system/bin/wpa_supplicant( 2790): ioctl[SIOCGIFFLAGS]: No such device
I//system/bin/wpa_supplicant( 2790): Could not get interface 'wlan0' flags
I//system/bin/wpa_supplicant( 2790): ioctl[SIOCSIWPMKSA]: No such device
I//system/bin/wpa_supplicant( 2790): ioctl[SIOCSIWMODE]: No such device
I//system/bin/wpa_supplicant( 2790): Could not configure driver to use managed mode
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/WifiHW  ( 2160): Unable to open connection to supplicant on "/data/system/wpa_supplicant/eth1": No such file or directory
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
D/dalvikvm( 2244): GC_EXPLICIT freed 6K, 49% free 2956K/5767K, external 4819K/6018K, paused 34ms
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
I/ActivityManager( 2160): Starting: Intent { act=android.intent.action.MAIN cmp=com.android.settings/.wifi.WifiSettings } from pid 2400
I/SurfaceFlinger( 2160): mHw->getFormat() 4
D/dalvikvm( 2400): GC_CONCURRENT freed 205K, 50% free 2961K/5831K, external 1167K/1619K, paused 3ms+4ms
I/ActivityManager( 2160): Displayed com.android.settings/.wifi.WifiSettings: +318ms
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/WifiHW  ( 2160): Unable to open connection to supplicant on "/data/system/wpa_supplicant/eth1": No such file or directory
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
E/WifiHW  ( 2160): Unable to open connection to supplicant on "/data/system/wpa_supplicant/eth1": No such file or directory
V/WifiStateTracker( 2160): Supplicant died unexpectedly
D/WifiStateTracker( 2160): Reset connections and stopping DHCP
E/wpa_supplicant( 2792): ioctl[SIOCGIWRANGE]
D/ConnectivityService( 2160): NetworkStateTracker.EVENT_STATE_CHANGED
D/ConnectivityService( 2160): ConnectivityChange for WIFI: DISCONNECTED/DISCONNECTED
D/WifiStateTracker( 2160): Disabling interface
D/NetworkStateTracker( 2160): setDetailed state, old =IDLE and new state=DISCONNECTED
D/Tethering( 2160): MasterInitialState.processMessage what=3
D/WifiStateTracker( 2160): Reset connections and stopping DHCP
D/WifiStateTracker( 2160): Disabling interface
D/dalvikvm( 2709): GC_EXPLICIT freed 110K, 54% free 2669K/5703K, external 716K/1038K, paused 32ms

0 Kudos
Reply

2,910 Views
waterzhou
Contributor V

what is error log? 

0 Kudos
Reply

2,910 Views
Swamy
Contributor III

We are using AR6103 SDIO interface on the SDCARD slot.

But when we connect it recognises the sdio card, but fails to connect.

Please suggest.

Regards,

Swamy

0 Kudos
Reply

2,911 Views
waterzhou
Contributor V

AR6103 is using hw2.1.1 firmware, so newer software release for ARD already support AR6103. Are you using AR6103 dongle?

0 Kudos
Reply