How to create custom SD card with custom kernel , uboot ,device tree , initramfs without touching the machine file.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to create custom SD card with custom kernel , uboot ,device tree , initramfs without touching the machine file.

1,851 次查看
harish_g
Contributor III

Our need is to create 2 seperate targets to create different image types for the same machine. Consider targets 'normal' and 'minimal' . When i use bitbake normal , the normal will generate the sdcard image with the default kernel , uboot , dtb and initramfs. But when i use bitbake minimal, this target should generate a sdcard image with a modified kernel,uboot ,dtb , initramfs. Is this acheivable without creating two seperate machine file versions.

I tried creating a new target following the 'mfgtool' path. But all mfgtool does is build required versions of the zImage,uboot,dtb,initramfs in the out directory and  call core-image.bbclass .When i try the same after removing FS types and other seemingly unrelated configurations, the custom zImage,uboot,dtb and initramfs gets built. But the default zImage,uboot and dtb still make it to the sdcard  image. 

Is there any way to specify which image should yocto consider as the actual zImage , uboot ,dtb and initramfs ? 

Rephrasing the question, Is there anyway to override building virtual/kernel and virtual/bootloader , without creating a completely seperate machine.conf file ?

标签 (2)
0 项奖励
回复
1 回复

1,562 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复