I couldn't find any ready to be used GPIO pins on MCIMX6SX-SDB, so I decided to break out some pins from SD2 connector which I am not currently using. What changes to the device tree do I need to make in order to use SD2_CMD, SD2_CLK, SD2_DATA0, SD2_DATA1, SD2_DATA2, SD2_DATA3 as GPIO?
I have already removed these sections from imx6sx-sdb.dtsi:
&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2>;
non-removable;
no-1-8-v;
keep-power-in-suspend;
wakeup-source;
status = "okay";
};
pinctrl_usdhc2: usdhc2grp {
fsl,pins = <
MX6SX_PAD_SD2_CMD__USDHC2_CMD 0x17059
MX6SX_PAD_SD2_CLK__USDHC2_CLK 0x10059
MX6SX_PAD_SD2_DATA0__USDHC2_DATA0 0x17059
MX6SX_PAD_SD2_DATA1__USDHC2_DATA1 0x17059
MX6SX_PAD_SD2_DATA2__USDHC2_DATA2 0x17059
MX6SX_PAD_SD2_DATA3__USDHC2_DATA3 0x17059
>;
};
I suppose now I need to add the definitions for the following pads:
But I'm not quite sure exactly how to do it. Could you please point me in the right direction?
解決済! 解決策の投稿を見る。
Hi Dima
one can try the same steps as for i.MX6UL
https://community.nxp.com/t5/i-MX-Processors/Simple-GPIO-Example-quandry/m-p/458731
Best regards
igor
Thank you very much for your answer, in my case the configuration value of 0x80000000 was sufficient, but GPIO on IMX processors is very flexible, I might return to this thread one day.
Hi Dima
one can try the same steps as for i.MX6UL
https://community.nxp.com/t5/i-MX-Processors/Simple-GPIO-Example-quandry/m-p/458731
Best regards
igor