How to correctly configure GPIO on imx6sx SABRE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to correctly configure GPIO on imx6sx SABRE?

跳至解决方案
1,596 次查看
itsemast
Contributor II

I couldn't find any ready to be used GPIO pins on MCIMX6SX-SDB, so I decided to break out some pins from SD2 connector which I am not currently using. What changes to the device tree do I need to make in order to use SD2_CMD, SD2_CLK, SD2_DATA0, SD2_DATA1, SD2_DATA2, SD2_DATA3 as GPIO?

I have already removed these sections from imx6sx-sdb.dtsi:

&usdhc2 {
       pinctrl-names = "default";
       pinctrl-0 = <&pinctrl_usdhc2>;
       non-removable;
       no-1-8-v;
       keep-power-in-suspend;
       wakeup-source;
       status = "okay";
};
		pinctrl_usdhc2: usdhc2grp {
			fsl,pins = <
				MX6SX_PAD_SD2_CMD__USDHC2_CMD		0x17059
				MX6SX_PAD_SD2_CLK__USDHC2_CLK		0x10059
				MX6SX_PAD_SD2_DATA0__USDHC2_DATA0	0x17059
				MX6SX_PAD_SD2_DATA1__USDHC2_DATA1	0x17059
				MX6SX_PAD_SD2_DATA2__USDHC2_DATA2	0x17059
				MX6SX_PAD_SD2_DATA3__USDHC2_DATA3	0x17059
			>;
		};

I suppose now I need to add the definitions for the following pads:

  • MX6SX_PAD_SD2_CMD__GPIO6_IO_7
  • MX6SX_PAD_SD2_CLK__GPIO6_IO_6
  • MX6SX_PAD_SD2_DATA0__GPIO6_IO_8
  • MX6SX_PAD_SD2_DATA1__GPIO6_IO_9
  • MX6SX_PAD_SD2_DATA2__GPIO6_IO_10
  • MX6SX_PAD_SD2_DATA3__GPIO6_IO_11

But I'm not quite sure exactly how to do it. Could you please point me in the right direction?

标签 (3)
标记 (1)
0 项奖励
回复
1 解答
1,588 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dima

 

one can try the same steps as for i.MX6UL

https://community.nxp.com/t5/i-MX-Processors/Simple-GPIO-Example-quandry/m-p/458731

 

Best regards
igor

 

在原帖中查看解决方案

2 回复数
1,576 次查看
itsemast
Contributor II

Thank you very much for your answer, in my case the configuration value of 0x80000000 was sufficient, but GPIO on IMX processors is very flexible, I might return to this thread one day.

0 项奖励
回复
1,589 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dima

 

one can try the same steps as for i.MX6UL

https://community.nxp.com/t5/i-MX-Processors/Simple-GPIO-Example-quandry/m-p/458731

 

Best regards
igor