Hi,
I have 4 1080p30fps MIPI CSI video streams and I would like to connect it to i.MX 8M plus processor. I think i.MX 8M Plus does not support virtual channel. I can only use i.MX 8M Processor as it is only one can do H.265 encoding. So
Thanks in advace for help and appricate time in answering.
I have 4 AHD cameras 1080p30, cant use IP Cameras, So I'm planning to use a conveter/decoder which can convert AHD video stream to IP and then feed it to i.mx 8m Plus? Do you have any solution to convter AHD to IP ?
Hi, Thanks for reply. I cant use imx8qm or imx8qxp as they are very expensive for my system and they cant do H.265 encoding in their VPUs.
So, regarding i.MX 8M Plus processor, how can I connect 4 MIPI CSI cameras without virtual channel support? is there any software way possible to implement?
Can i.MX 8M plus processor do H.265 encoding for 4 Video streams in real time. Its VPU is capable of doing H.265 encoding but I'm concerned about encoding 4 video streams 1080p30?
Thanks