How to configure/use tc358743 hdmi->mipi by gstreamer and v4l2-ctl

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure/use tc358743 hdmi->mipi by gstreamer and v4l2-ctl

1,617件の閲覧回数
lmtan91
Contributor II

Hi,

 
Below is log when run 'media-ctl -p'

 

 

media-ctl -p

Media controller API version 5.10.52

Media device information
------------------------
driver          imx7-csi
model           imx-media
serial          
bus info        
hw revision     0x0
driver version  5.10.52

Device topology
- entity 1: csi (2 pads, 2 links)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev0
        pad0: Sink
                [fmt:UYVY8_2X8/800x600 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                <- "imx7-mipi-csis.0":1 []
        pad1: Source
                [fmt:UYVY8_2X8/800x600 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
                -> "csi capture":0 []

- entity 4: csi capture (1 pad, 1 link)
            type Node subtype V4L flags 0
            device node name /dev/video2
        pad0: Sink
                <- "csi":1 []

- entity 10: imx7-mipi-csis.0 (2 pads, 2 links)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev1
        pad0: Sink
                [fmt:UYVY8_2X8/640x480 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                <- "tc358743 0-000f":0 []
        pad1: Source
                [fmt:UYVY8_2X8/640x480 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
                -> "csi":0 []

- entity 15: tc358743 0-000f (1 pad, 1 link)
             type V4L2 subdev subtype Unknown flags 0
             device node name /dev/v4l-subdev2
        pad0: Source
                [fmt:RGB888_1X24/640x480 field:none colorspace:srgb]
                [dv.caps:BT.656/1120 min:640x350@13000000 max:1920x1200@165000000 stds:CEA-861,DMT,CVT,GTF caps:progressive,reduced-blanking,custom]
                [dv.query:no-link]
                [dv.current:BT.656/1120 640x480p59 (800x525) stds:CEA-861,DMT flags:has-cea861-vic]
                -> "imx7-mipi-csis.0":0 []

 

 

 

But when I run gstreamer, it failed

 

 

gst-launch-1.0 v4l2src device=/dev/video2 ! 'video/x-raw, format=(string)UYVY,width=800,height=600,framerate=(fraction)30/1' ! queue ! jpegenc ! multipartmux ! tcpserversink host=0.0.0.0 port=1223

 

 

Log

 

 

Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.
Additional debug info:
../git/libs/gst/base/gstbasesrc.c(3127): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason not-negotiated (-4)
Execution ended after 0:00:00.000414915
Setting pipeline to NULL ...
Freeing pipeline ...

 

 

 

I enabled GST_DEBUG level 4, the log as attached: gstreamer_log.txt

 

Could you please review and support me on this?

 

Best regards,

Tan

 

 

タグ(3)
0 件の賞賛
返信
0 返答(返信)