Dear Support,
I am trying to setup the registers of the video processing chain with a ov9732 sensor as the source.
The path is following:
ov9732 -> mipi/csi-2 -> csi/ipu gasket -> csi input -> sfmc -> idmac -> memory
The source can only be configured in this mode V4L2_IF_TYPE_BT656_MODE_BT_10BIT.
When storing in 16-bit format into memory, the images are good.
But when enabling the compander in the ipu to produce a 8-bit format, the images are noisy.
What is the proper IPU registers setup to get the bayer 8-bit per pixel format working?
The linux version is: 4.1.15-1.0.0 build using yocto.
Attached is a bayer BGGR image which can be visualized in 8-bit grey scale.
Below are some logs showing the content of registers:
setup_ifparm,1491: csi_param: vsync_pol(0) hsync_pol(0) ext_vsync(0)
ipu_csi_init_interface,104: setting cfg_param.data_fmt CSI_SENS_CONF_DATA_FMT_BAYER
ioctl_g_ifparm,777: u.bt656.mode 4, V4L2_IF_TYPE_BT656_MODE_BT_10BIT
setup_ifparm,1468: ifparm.u.bt656.clock_curr=22000000
setup_ifparm,1473: csi_param.clk_mode=1
setup_ifparm,1482: csi_param.data_width=IPU_CSI_DATA_WIDTH_10
setup_ifparm,1485: csi_param.pack_tight=0
setup_ifparm,1491: csi_param: vsync_pol(0) hsync_pol(0) ext_vsync(0)
csi_enc_setup,89:, sensor_protocol 1
csi_enc_setup,119: setting pixel_fmt = IPU_PIX_FMT_GENERIC
csi_enc_setup,145: pixel_fmt IPU0
csi_enc_setup,146: v2f.fmt.pix.pixelformat BA81
_ipu_csi_init,940: Enabling 10-bit to 8-bit companding
CSI_SENS_CONF = 0x00001b10
CSI_SENS_FRM_SIZE = 0x02cf04ff
CSI_ACT_FRM_SIZE = 0x02cf04ff
CSI_OUT_FRM_CTRL = 0x00000000
CSI_TST_CTRL = 0x00000000
CSI0_CPD_CTRL = 0x00000010
CSI1_CPD_CTRL = 0x00000000
CSI_CPD_OFFSET1 = 0x00000000
CSI_CPD_OFFSET2 = 0x00000000
CSI_CPD_RC((0)) = 0x00200000
CSI_CPD_GRC((0)) = 0x00200000
CSI_CPD_GBC((0)) = 0x00200000
CSI_CPD_BC((0)) = 0x00200000
CSI_CPD_RC((1)) = 0x00600040
CSI_CPD_GRC((1)) = 0x00600040
CSI_CPD_GBC((1)) = 0x00600040
CSI_CPD_BC((1)) = 0x00600040
CSI_CPD_RC((2)) = 0x00a00080
CSI_CPD_GRC((2)) = 0x00a00080
CSI_CPD_GBC((2)) = 0x00a00080
CSI_CPD_BC((2)) = 0x00a00080
CSI_CPD_RC((3)) = 0x00e000c0
CSI_CPD_GRC((3)) = 0x00e000c0
CSI_CPD_GBC((3)) = 0x00e000c0
CSI_CPD_BC((3)) = 0x00e000c0
CSI_CPD_RC((4)) = 0x01200100
CSI_CPD_GRC((4)) = 0x01200100
CSI_CPD_GBC((4)) = 0x01200100
CSI_CPD_BC((4)) = 0x01200100
CSI_CPD_RC((5)) = 0x01600140
CSI_CPD_GRC((5)) = 0x01600140
CSI_CPD_GBC((5)) = 0x01600140
CSI_CPD_BC((5)) = 0x01600140
CSI_CPD_RC((6)) = 0x01a00180
CSI_CPD_GRC((6)) = 0x01a00180
CSI_CPD_GBC((6)) = 0x01a00180
CSI_CPD_BC((6)) = 0x01a00180
CSI_CPD_RC((7)) = 0x01e001c0
CSI_CPD_GRC((7)) = 0x01e001c0
CSI_CPD_GBC((7)) = 0x01e001c0
CSI_CPD_BC((7)) = 0x01e001c0
CSI_CPD_RS((0)) = 0x20202020
CSI_CPD_GRS((0)) = 0x20202020
CSI_CPD_GBS((0)) = 0x20202020
CSI_CPD_BS((0)) = 0x20202020
CSI_CPD_RS((1)) = 0x20202020
CSI_CPD_GRS((1)) = 0x20202020
CSI_CPD_GBS((1)) = 0x20202020
CSI_CPD_BS((1)) = 0x20202020
CSI_CPD_RS((2)) = 0x20202020
CSI_CPD_GRS((2)) = 0x20202020
CSI_CPD_GBS((2)) = 0x20202020
CSI_CPD_BS((2)) = 0x20202020
CSI_CPD_RS((3)) = 0x20202020
CSI_CPD_GRS((3)) = 0x20202020
CSI_CPD_GBS((3)) = 0x20202020
CSI_CPD_BS((3)) = 0x20202020
ipu_init_channel, 839: csi 0, channel 268435392, Calling _ipu_csi_init: params->csi_mem.mipi.en 1
ipu_init_channel_buffer,1461: channel=268435392, type=0, pixel_fmt=0x30555049, width=1280, height=720, stride=120
ipu_init_channel_buffer,1467: phyaddr_0 = 0x40800000, phyaddr_1 = 0x40800000, phyaddr_2 = 0x00000000, u=0, v=0
initializing idma ch 0 @ c08c0000
ipu_init_channel_buffer, 1560: reading burst_size 64
ipu_init_channel_buffer, 1569: IPU_PIX_FMT_GENERIC: setting SMFC burst_size 4
ch 0 word 0 - 00000000 00000000 00000000 E0002800 000B3C9F
ch 0 word 1 - 08100000 01020000 00CFC000 00013FC0 00000000
PFS 0x6,
BPP 0x5, NPB 0x3f
FW 1279,
FH 719, EBA0 0x40800000
EBA1 0x40800000
Stride 1279
scan_order 0
uv_stride 0
u_offset 0x0
v_offset 0x0
Width0 0+1,
Width1 0+1, Width2 0+1,
Width3 0+1, Offset0 0,
Offset1 0, Offset2 0,
Offset3 0
Looked into FCW format converter write and forced the following values to CPMEM for the given channel (0):
- BPP: 0 (32-bit per pixel)
- PFS: RGB (although the data is generic, packing only works with PFS=7, see table 38-14. Channel Parameters Memory for interleaved, i.MX6DL RM rev. 3, 09/207)
- NBP: 15 (burst size 16)
I am hoping to get rid of the 8-bit LSB of a 16-bit word coming out of CSI as generic data without using the compander.
Defined width0 to width3 and offset 0 to offset3 using the following function:
_ipu_ch_params_set_packing(¶ms, 3, 0, 3, 4, 3, 16, 3, 20);
I also tried with BPP = 3 (16-bit per pixel) and burst size 32 and
_ipu_ch_params_set_packing(¶ms, 1, 0, 1, 2, 1, 4, 1, 6);
But have no success, the image looks like if bursts of data are repeated three times.
Any solution which would work with generic data?
some IPU packing examples one can find in Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK
Thanks Igor,
I have been looking at function ipu_idma_pixel_format_config() in file ipu_idmac.c, how two RGB formats are packed.
By setting following values, I now get an image that is duplicated vertically and horizontally.
BPP: 5 (8-bit)
NPB: 7 (idmac burst size of 8, any value different from this results in a noisy picture)
BPF: 7 (RGB)
Packing: _ipu_ch_params_set_packing(¶ms, 8, 0, 8, 8, 8, 16, 8, 24);
I would expect idmac to write only the byte at offset 0 to memory. Is this really the case?
SMFC burst size does not seem to have an impact. What should be the correct setting here?
Hi Brigitte
one can also look in sect.18.10.1.4 Configuring the DC block
iMX6_Firmware_Guide.pdf included in SDK. Bayer sensors are not
supported in NXP official BSPs, so there are no validated or recommended settings.
Best regards
igor
Hi Igor,
This section refers to the display path of the IPU and does not seem to apply to the capture path at all. It raises a question though, is there a specific firmware for the IPU capture side? If yes, what should be the latest version?
Thanks,
Brigitte
Hi Brigitte
please check nxp official linux documentation on
Documentation describes software features which are "officially" supported:
that is tested and documented. All other sw efforts which are not listed in documentation,
such as custom drivers, can be supported using Professional Service
Best regards
igor
Hi Brigitte
unfortunately IPU does not support natively bayer format, may be useful to check below links
IPU - bayer pattern conversion
https://community.nxp.com/message/344529#344529
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor, I am not sure I understand your answer correctly.
Per the reference manual, the IPU cannot convert a Bayer format to RGB or YUV which is OK.
But I expect the IPU to be able to transfer Bayer data from the sensor to memory properly.
The only difference here with other applications is that the sensor provides 10-bit raw data that IPU is supposed to quantize down to 8-bit using the compander and store as 8-bit into memory.
Are you saying this is not going to work?
IPU does not "know" about Bayer format, there is no special processing for that format.
For packing capabilities one can look at sect.37.4.2.3 FCW & FCR - Format converter
write and read i.MX6DQ Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor